![]() |
PDK API Guide for J721E
|
Input args for CPSW_ALE_IOCTL_SET_POLICER command.
Data Fields | |
CpswAle_PolicerMatchParams | policerMatch |
bool | threadIdEn |
uint32_t | threadId |
uint32_t | peakRateInBitsPerSec |
uint32_t | commitRateInBitsPerSec |
CpswAle_PolicerMatchParams CpswAle_SetPolicerEntryInArgs::policerMatch |
Policer match config
bool CpswAle_SetPolicerEntryInArgs::threadIdEn |
Enable threadid setting for this policer entry
uint32_t CpswAle_SetPolicerEntryInArgs::threadId |
Thread Id which will be enabled for this policer match
uint32_t CpswAle_SetPolicerEntryInArgs::peakRateInBitsPerSec |
Peak rate in bits per second. 0 indicates rate limit is disabled
uint32_t CpswAle_SetPolicerEntryInArgs::commitRateInBitsPerSec |
Commit rate in bits per second. 0 indicates rate limit is disabled