PDK API Guide for J721E
|
Functions | |
static void | EnetDma_checkPktState (uint32_t *pStateVar, EnetDma_PktStateModuleType module, uint32_t expectedState, uint32_t newState) |
Packet state check & set API for app, memory manager and dma driver. More... | |
static void | EnetDma_checkDescState (uint32_t *pStateVar, EnetDma_DescStateMemMgr expectedState, EnetDma_DescStateMemMgr newState) |
Descriptor state check & set API for descriptor memory manager. More... | |
Enumerations | |
enum | EnetDma_DescStateMemMgr { ENET_DESCSTATE_MEMMGR_FREE = 0U, ENET_DESCSTATE_MEMMGR_ALLOC } |
Enet DMA Descriptor state. More... | |
enum | EnetDma_PktStateApp { ENET_PKTSTATE_APP_WITH_FREEQ = 0U, ENET_PKTSTATE_APP_WITH_READYQ, ENET_PKTSTATE_APP_WITH_DRIVER } |
App Pkt state. More... | |
enum | EnetDma_PktStateDma { ENET_PKTSTATE_DMA_WITH_HW = 0U, ENET_PKTSTATE_DMA_NOT_WITH_HW } |
DMA Pkt state. More... | |
enum | EnetDma_PktStateMemMgr { ENET_PKTSTATE_MEMMGR_FREE = 0U, ENET_PKTSTATE_MEMMGR_ALLOC } |
Enet DMA Pkt state. More... | |
enum | EnetDma_PktStateModuleType { ENET_PKTSTATE_MODULE_APP = 0U, ENET_PKTSTATE_MODULE_DRIVER, ENET_PKTSTATE_MODULE_MEMMGR } |
Enet DMA Pkt state. More... | |
Macros | |
#define | ENET_UTILS_GET_STATE(state, mask, bitshift) ((*(state) & (mask)) >> (bitshift)) |
#define | ENET_UTILS_SET_STATE(state, mask, bitshift, value) |
#define | ENET_UTILS_DRIVER_STATE_MASK (0x000000FFU) |
#define | ENET_UTILS_DRIVER_STATE_BIT_SHIFT (0U) |
#define | ENET_DMA_MEMMGR_STATE_MASK (0x0000FF00U) |
#define | ENET_DMA_MEMMGR_STATE_BIT_SHIFT (8U) |
#define | ENET_UTILS_APP_STATE_MASK (0x00FF0000U) |
#define | ENET_UTILS_APP_STATE_BIT_SHIFT (16U) |
#define | ENET_UTILS_GET_PKT_DRIVER_STATE(state) |
#define | ENET_UTILS_SET_PKT_DRIVER_STATE(state, value) |
#define | ENET_UTILS_GET_PKT_MEMMGR_STATE(state) |
#define | ENET_UTILS_SET_PKT_MEMMGR_STATE(state, value) |
#define | ENET_UTILS_GET_PKT_APP_STATE(state) |
#define | ENET_UTILS_SET_PKT_APP_STATE(state, value) |
#define | ENET_DMA_MEMMGR_DESCSTATE_MASK (0x000000FFU) |
#define | ENET_DMA_MEMMGR_DESCSTATE_SHIFT (0U) |
#define | ENET_UTILS_GET_DESC_MEMMGR_STATE(state) |
#define | ENET_UTILS_SET_DESC_MEMMGR_STATE(state, value) |
#define ENET_UTILS_DRIVER_STATE_MASK (0x000000FFU) |
#define ENET_UTILS_DRIVER_STATE_BIT_SHIFT (0U) |
#define ENET_DMA_MEMMGR_STATE_MASK (0x0000FF00U) |
#define ENET_DMA_MEMMGR_STATE_BIT_SHIFT (8U) |
#define ENET_UTILS_APP_STATE_MASK (0x00FF0000U) |
#define ENET_UTILS_APP_STATE_BIT_SHIFT (16U) |
#define ENET_UTILS_GET_PKT_DRIVER_STATE | ( | state | ) |
#define ENET_UTILS_GET_PKT_MEMMGR_STATE | ( | state | ) |
#define ENET_UTILS_GET_PKT_APP_STATE | ( | state | ) |
#define ENET_DMA_MEMMGR_DESCSTATE_MASK (0x000000FFU) |
#define ENET_DMA_MEMMGR_DESCSTATE_SHIFT (0U) |
#define ENET_UTILS_GET_DESC_MEMMGR_STATE | ( | state | ) |
enum EnetDma_PktStateApp |
enum EnetDma_PktStateDma |
|
inlinestatic |
Packet state check & set API for app, memory manager and dma driver.
This development time API checks expected state and sets new packet state. This is used by modules handling the packet to confirm the packet is returned and allocated in correct state. Memutils checks (free, allocated), dma driver checks (with Hw, with driver) and app checks which queue it belongs
pStateVar | [IN/OUT] Pointer to packet state variable of packet structure EnetDma_Pkt |
module | [IN] Module id. Refer to EnetDma_PktStateModuleType |
expectedState | [IN] State packet is expected to be. |
newState | [IN] New state packet is set to. |
|
inlinestatic |
Descriptor state check & set API for descriptor memory manager.
This development time API checks expected state and sets new descriptor state. This is used by modules handling the Desc to confirm the Desc is returned and allocated in correct state. Only memutils modules uses it now for checking if desc is free or allocated while allocating or freeing desc respectively.
pStateVar | [IN/OUT] Pointer to Desc state variable. |
expectedState | [IN] State Desc is expected to be. |
newState | [IN] New state Desc is set to. |