PDK API Guide for J721E
|
This is UDMA driver common parameters and API
Files | |
file | udma_types.h |
UDMA Low Level Driver API/interface data types file. | |
Macros | |
#define | UDMA_CACHELINE_ALIGNMENT (128U) |
Cache line size for alignment of descriptor and buffers. More... | |
#define | UDMA_NO_WAIT ((uint32_t) 0U) |
UDMA transaction timeout define - no wait. More... | |
#define | UDMA_WAIT_FOREVER (~((uint32_t) 0U)) |
UDMA transaction timeout define - wait for ever. More... | |
#define | UDMA_INIT_DONE (0xABDCABCDU) |
Macro used to specify that init is performed for an object. More... | |
#define | UDMA_DEINIT_DONE (0x00000000U) |
Macro used to specify that deinit is performed for an object. More... | |
UDMA Error Codes | |
Error codes returned by UDMA APIs | |
#define | UDMA_SOK (CSL_PASS) |
API call successful. More... | |
#define | UDMA_EFAIL (CSL_EFAIL) |
API call returned with error as failed. Used for generic error. It may be some hardware failure and/or software failure. More... | |
#define | UDMA_EBADARGS (CSL_EBADARGS) |
API call returned with error as bad arguments. Typically, NULL pointer passed to the API where its not expected. More... | |
#define | UDMA_EINVALID_PARAMS (CSL_EINVALID_PARAMS) |
API call returned with error as invalid parameters. Typically when parameters passed are not valid or out of range. More... | |
#define | UDMA_ETIMEOUT (CSL_ETIMEOUT) |
API call returned with error as timed out. Typically API is waiting for some condition and returned as condition not happened in the timeout period. More... | |
#define | UDMA_EALLOC (CSL_EALLOC) |
API call returned with error as allocation failed. More... | |
UDMA Instance ID | |
This represents the various Instances in an SOC. The actual Instances present in the chip is SOC dependent. Refer soc file for the actual instance present. Kindly use Udma_InstanceIdSoc macros for SOC specific name. | |
#define | UDMA_INST_ID_0 (0U) |
#define | UDMA_INST_ID_1 (1U) |
#define | UDMA_INST_ID_2 (2U) |
#define | UDMA_INST_ID_3 (3U) |
UDMA UTC ID | |
This represents the various UTC IP in the SOC. The actual UTC present in the chip is SOC dependent. Refer soc file for the actual instance present. Kindly use Udma_UtcIdSoc macros for SOC specific name. | |
#define | UDMA_UTC_ID0 (0U) |
#define | UDMA_UTC_ID1 (1U) |
#define | UDMA_UTC_ID2 (2U) |
#define | UDMA_UTC_ID3 (3U) |
#define | UDMA_UTC_ID4 (4U) |
#define | UDMA_UTC_ID5 (5U) |
#define | UDMA_UTC_ID6 (6U) |
#define | UDMA_UTC_ID7 (7U) |
#define | UDMA_UTC_ID8 (8U) |
#define | UDMA_UTC_ID9 (9U) |
UDMA Mapped Group | |
This represents the various Mapped TX & RX Channels/Rings in the SOC. The actual Mapped TX & RX groups present in the chip is SOC dependent. Refer soc file for the actual instance present. Kindly use Udma_MappedTxGrpSoc macros for Mapped TX SOC specific name and Udma_MappedRxGrpSoc macros for Mapped RX SOC specific name. | |
#define | UDMA_MAPPED_GROUP0 (0U) |
#define | UDMA_MAPPED_GROUP1 (1U) |
#define | UDMA_MAPPED_GROUP2 (2U) |
#define | UDMA_MAPPED_GROUP3 (3U) |
#define | UDMA_MAPPED_GROUP4 (4U) |
#define | UDMA_MAPPED_GROUP5 (5U) |
#define | UDMA_MAPPED_GROUP6 (6U) |
#define | UDMA_MAPPED_GROUP7 (7U) |
#define UDMA_CACHELINE_ALIGNMENT (128U) |
Cache line size for alignment of descriptor and buffers.
#define UDMA_SOK (CSL_PASS) |
API call successful.
#define UDMA_EFAIL (CSL_EFAIL) |
API call returned with error as failed. Used for generic error. It may be some hardware failure and/or software failure.
#define UDMA_EBADARGS (CSL_EBADARGS) |
API call returned with error as bad arguments. Typically, NULL pointer passed to the API where its not expected.
#define UDMA_EINVALID_PARAMS (CSL_EINVALID_PARAMS) |
API call returned with error as invalid parameters. Typically when parameters passed are not valid or out of range.
#define UDMA_ETIMEOUT (CSL_ETIMEOUT) |
API call returned with error as timed out. Typically API is waiting for some condition and returned as condition not happened in the timeout period.
#define UDMA_EALLOC (CSL_EALLOC) |
API call returned with error as allocation failed.
#define UDMA_NO_WAIT ((uint32_t) 0U) |
UDMA transaction timeout define - no wait.
#define UDMA_WAIT_FOREVER (~((uint32_t) 0U)) |
UDMA transaction timeout define - wait for ever.
#define UDMA_INIT_DONE (0xABDCABCDU) |
Macro used to specify that init is performed for an object.
#define UDMA_DEINIT_DONE (0x00000000U) |
Macro used to specify that deinit is performed for an object.
#define UDMA_INST_ID_0 (0U) |
#define UDMA_INST_ID_1 (1U) |
#define UDMA_INST_ID_2 (2U) |
#define UDMA_INST_ID_3 (3U) |
#define UDMA_UTC_ID0 (0U) |
#define UDMA_UTC_ID1 (1U) |
#define UDMA_UTC_ID2 (2U) |
#define UDMA_UTC_ID3 (3U) |
#define UDMA_UTC_ID4 (4U) |
#define UDMA_UTC_ID5 (5U) |
#define UDMA_UTC_ID6 (6U) |
#define UDMA_UTC_ID7 (7U) |
#define UDMA_UTC_ID8 (8U) |
#define UDMA_UTC_ID9 (9U) |
#define UDMA_MAPPED_GROUP0 (0U) |
#define UDMA_MAPPED_GROUP1 (1U) |
#define UDMA_MAPPED_GROUP2 (2U) |
#define UDMA_MAPPED_GROUP3 (3U) |
#define UDMA_MAPPED_GROUP4 (4U) |
#define UDMA_MAPPED_GROUP5 (5U) |
#define UDMA_MAPPED_GROUP6 (6U) |
#define UDMA_MAPPED_GROUP7 (7U) |