Logsp
Detailed Description
Function Documentation
- Description:
- The logsp function returns the logarithm function of a real floating-point argument a. The return value is the base e logarithmic value of a.
- Parameters:
-
- Returns:
- Resultant float
- Special Cases:
- If a is Inf, the return value is 88.99999 (Asm) or 709.7827 (C/Inline/Vector).
- See also:
-
- Implementation Notes:
- The code supports both big and little endian modes.
| float logsp_c |
( |
float |
a |
) |
|
Copyright 2016, Texas Instruments Incorporated