Collaboration diagram for DSPF_sp_maxidx:
int | DSPF_sp_maxidx (const float *x, const int nx) |
int DSPF_sp_maxidx | ( | const float * | x, | |
const int | nx | |||
) |
This routine finds out the index of maximum number in the input array. This function returns the index of the greatest value.
x | Pointer to input array. | |
nx | Number of inputs in the input array. |