Collaboration diagram for DSPF_sp_lud_solver_cmplx:
int | DSPF_sp_lud_solver_cmplx (const int order, unsigned short *restrict P, float *restrict L, float *restrict U, float *restrict b, float *restrict b_mod, float *restrict y, float *restrict x) |
int DSPF_sp_lud_solver_cmplx | ( | const int | order, | |
unsigned short *restrict | P, | |||
float *restrict | L, | |||
float *restrict | U, | |||
float *restrict | b, | |||
float *restrict | b_mod, | |||
float *restrict | y, | |||
float *restrict | x | |||
) |
This function solves the system of linear equations A*x=b for x using the inputs produced by DSPF_sp_lud where A*x=transpose(P)*L*U*x=b. The following procedure is performed.
1. Modify b using permutation matrix: b_mod = L*U*x = P*b
2. Use forward substitution to solve for y: y = U*x = inv(L)*b_mod
3. Use backward substitution for solve for x: x = inv(U)*y
The values stored in the matrices are assumed to be float precision floating point values. This code is suitable for dense matrices. No optimizations are made for sparse matrices.
Nrows | = number of rows in square complex matrix A | |
P | = pointer to permutation matrix P[Nrows*Nrows] | |
L | = pointer to lower triangular matrix complex L[2*Nrows*Nrows] | |
U | = pointer to upper triangular matrix complex U[2*Nrows*Nrows] | |
b | = pointer to complex vector b[2*Nrows] | |
b_mod | = pointer to modified complex vector b_mod[2*Nrows] | |
y | = pointer to temporary complex vector y[2*Nrows] | |
x | = pointer to final solver output complex vector x[2*Nrows] |