2.7. Release Notes - 07_00_00¶
2.7.1. Introduction¶
This release notes provides important information that will assist you in using the PDK software package. This document provides the product information and known issues that are specific to the PDK software package.
2.7.2. What’s New¶
ID | Description | Module |
---|---|---|
PDK-4940 | SBL shall program the Thermal shutdown (TSHUT) values during boot | SBL |
PDK-5246 | Boot time Security support on RTOS SDK for AM65xx and J721E Platforms | SBL |
PDK-6298 | SciClient: Update the Sciclient_rmIrqSet and Sciclient_rmIrqRelease APIs to perform interrupt routing | Sciclient |
PDK-5264 | Support Thumb2 mode on R5F | BUILD |
PDK-5372 | Board: DDR software shall use EMIF/LPDDR chip support library | BOARD |
PDK-5367 | DDR software shall support runtime refresh rate modification based on temperature feedback | BOARD |
PDK-5866 | VTM: SW shall enable configuration of Temperature Warning | CSL VTM |
PDK-5366 | CSL-FL: FSS Support | CSL FSS |
PDK-5149 | Support DSS, VHWA, CSI-RX, CSI-TX on mcu2_0 instead of mcu2_1 | Video Drivers |
PDK-5252 | AM65xx PG2: CAL Configuration option to route traffic through real time or non real time path | CAL |
PDK-5204 | Fusion 2 board Support | CSIRX |
PDK-5255 | CSIRX: YUV422 dataformat Support | CSIRX |
PDK-5253 | CSI2 TX : Support for multiple virtual channel | CSITX |
PDK-4988 | AM65xx PG2: DSS Driver update required to support yuv2rgb | DSS |
PDK-6486 | VPAC LDC driver shall support config updates after create time | VPAC |
PDK-5811 | PMIC: Driver shall support TPS6594x (Leo) | PMIC |
PDK-4966 | SA2UL Driver shall be supported | SA2UL |
ETHFW-1201 | CPSW Checksum offload support | CPSW |
ETHFW-1163 | Directed packet support | CPSW |
ETHFW-1139 | Tx packet control: Timestamp Enable, Domain, msg_type, sequence_id | CPSW |
2.7.2.1. SBL¶
- Adds J721E-HS secure boot support for RTOS SDK
- Programs thermal limits for J721E to force the SoC into reset if the max temp is reached
- SBL “cust” build by default now only initializes MCU DOMAIN clocks & resources for a faster boot option for MCU R5 apps (J721E/J721E-HS only)
- Added an optional set of build flags for the SBL “cust” build specifically for testing Early CAN response
- Added a small-footprint SBL boot performance test app that works with the SBL “cust” build (MCU DOMAIN only usage)
- Optional SBL build flag added to allow subsequent software (e.g., HLOS) to take control of the OSPI flash
- Updated the default GTC clock rate to 200 MHz. Matches the value expected by ARM Trusted Firmware build for the Cortex-A cores.
- SBL update added to fix occasional instability seen when the R5 reads from the OSPI flash
2.7.2.2. SYSFW¶
- Security Features:
- Official support for silicon tested J721e HS images.
- HS Devices: Support for configuring derived KEK (DKEK) in SA2UL and enabled host access to SA2UL
- Removed support of HSM-related features (TRNG, Asymmetric key services, and keystore)
- Global soft lock for extended OTP
- PM Features:
- HW PTSTAT silicon errata workaround
- RM Features:
- RM board configuration now allows up to two assignments of a resource per host.
- Added the TISCI_MSG_RM_UDMAP_FLOW_DELEGATE message to pass configuration control of common flows to other hosts.
- Boot Time Optimizations
- SYSFW Boot notification + Board Configuration = 6.39 ms (Within Budget of 5 ms (+/- 2 ms))
- ROM MCU Only Boot mode support.
2.7.3. Upgrade and Compatibility¶
2.7.3.1. Build and Packaging¶
The PDK Jacinto package is now a combined package for both AM65xx and J721E platforms. Hence the pdk folder name in SDK reflect the family name rather than the SOC name like am65xx or j721e. Due to this the PDK_SOC variable derived from the pdk folder while sourcing pdksetupenv.sh/.bat will default to one of the SOC in the family i.e. in this case am65xx
- This means user need to set PDK_SOC variable to the required SOC while calling pdk makefile from PDK_INSTALL_DIR/packages
Only the files applicable to a particular platform is packaged. This is to done to reduce the overall package size, remove unwanted files for users for better file/folder navigation and also to ensure that a file which is not applicable for a platform is not wrongly included by application
- Due to this some of the application interface files may be missing from the package compared to last release. Users are advised to remove the inclusion of these files in their application for the respective platform builds
API guide for PDK is now generated for the entire PDK package instead of individual module API guides. The generated API guide is now present in PDK_INSTALL_DIR/docs/api_guide folder. This gives flexibility to give cross references across modules in PDK as well generate SOC specific documentation. Due to this API_Documentation.html present in PDK_INSTALL_DIR/packages is removed
2.7.3.2. CPSW¶
Hardware push instance number in CPTS events is now an enumeration of type CpswCpts_HwPush, not an 8-bit integer.
CPSW DMA TX channel params (CpswDma_UdmaChTxPrms) added boolean flags to filter out extended and protocol specific info words.
- Exposed below UDMA ring and channel config params
- Added Ring mode config option in CpswDma_UdmaRingPrms
- CpswDma_UdmaFlowPrms - added boolean flags to indicate if extended or protocol specific info words.
CpswDma_PktInfo now has fields for packet timestamp information (CpswDma_PktTsInfo) and directed port numbers.
2.7.3.3. SBL¶
- In case of AM65xx-HS build, the HS SBL image is generated under PDK_INSTALL_DIR/packages/ti/boot/sbl/binary/am65xx_evm_hs folder instead of PDK_INSTALL_DIR/packages/ti/boot/sbl/binary/am65xx_evm folder. This is done in order to support HS and GP builds in the same package.
- In case of HS build, BUILD_HS flag need not be passed while calling make. Both the HS and GP SBL binaries gets generated by the default build procedures
2.7.3.4. Sciclient¶
Due to a System Firmware ABI change, applications using the Sciclient_rmGetResourceRange API to retrieve host processor IRQ ranges need to update the processor through which processor IRQ ranges are discovered.
System Firmware no longer directly manages host processor input IRQs as a resource. All resources of subtype TISCI_RESASG_SUBTYPE_<destination processor IRQ interface>_IRQ_GROUPr*_FROM_<source interrupt router> have been removed.
System Firmware now manages all interrupt router (IR) outputs directly with SoC IR output ranges managed under the resource subtype TISCI_RESASG_SUBTYPE_IR_OUTPUT
Applications that query System Firmware for the host processor input IRQ range via the Sciclient_rmGetResourceRange() must update the types and subtypes used in the query. The processor IRQ subtypes have been removed. The query via Sciclient_rmGetResourceRange() now needs to use SoC IR types and the IR output resource subtype. Note, this requires knowledge of which IR is directly connected to the processor IRQ input range desired for configuration. The linked tables below show the resource type migration that an application using the Sciclient_rmGetResourceRange() API should make when switching from the old IRQ input resource types to the new IR output resource types.
To facilitate backwards compatibility between the new IR output resource and the Sciclient_rmIrqSet and Sciclient_rmIrqRelease APIs which take a destination host IRQ (dst_host_irq parameter) as input the Sciclient_rmIrqTranslateIrOutput() API has been added.
The Sciclient_rmIrqTranslateIrOutput API translates an IR output to the destination processor input IRQ value. The returned value can be provided directly to the dst_host_irq parameter of the Sciclient_rmIrqSet and Sciclient_rmIrqRelease APIs.
New Sciclient_rmIrqSetRaw and Sciclient_rmIrqReleaseRaw APIs have been added. These APIs allow direct programming of SoC interrupt aggregators (IA) and interrupt routers (IR) in accordance to new System Firmware interrupt management functionality.
The existing Sciclient_rmIrqSet and Sciclient_rmIrqRelease APIs continue to function as they did before.
2.7.3.5. SYSFW¶
- Interrupt management Simplification and Memory Optimization. (ABI 3.0)
- Board configuration updates for New Security features - DKEK, SA2UL sharing. (ABI 3.0)
- AM65x SR 1.0 RM resource assignment types are now aligned with AM65x SR 2.0 resource assignment types
- The TISCI_MSG_RM_GET_RESOURCE_RANGE has been updated to return an additional resource range - Backward compatible.
2.7.3.6. Executing sysbios applications via CCS (no-boot mode)¶
- An additional step of copying interrupt vector to ATCM is necessary
- Refer FAQ Copy Vecs to ATCM for details
2.7.3.7. BOARD Diagnostics¶
- In case of AM65xx, the board diagnostics builds are now supported from PDK top level makefile present in pdk/packages/makefile or from pdk/packages/ti/build folders
- Board diagnostic application image location is changed from ‘pdk/packages/ti/board/bin’ to ‘pdk/packages/binary’. Refer to Board Diagnostics Documentation for more details.
2.7.3.7.1. AM65X Sciclient Interrupt Resource Type Migration Table¶
Old Resource Type | Old Resource Subtype | New Resource Type | New Resource Subtype |
---|---|---|---|
RESASG_TYPE_GIC_IRQ | RESASG_SUBTYPE_GIC_IRQ_MAIN_NAV_SET0 | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
RESASG_SUBTYPE_GIC_IRQ_MAIN_GPIO | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
RESASG_SUBTYPE_GIC_IRQ_MAIN_NAV_SET1 | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
RESASG_SUBTYPE_GIC_IRQ_COMP_EVT | TISCI_DEV_CMPEVENT_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
RESASG_SUBTYPE_GIC_IRQ_WKUP_GPIO | TISCI_DEV_WKUP_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
RESASG_TYPE_PULSAR_C0_IRQ | RESASG_SUBTYPE_PULSAR_C0_IRQ_MCU_NAV | TISCI_DEV_MCU_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
RESASG_SUBTYPE_PULSAR_C0_IRQ_WKUP_GPIO | TISCI_DEV_WKUP_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
RESASG_SUBTYPE_PULSAR_C0_IRQ_MAIN2MCU_LVL | TISCI_DEV_MAIN2MCU_LVL_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
RESASG_SUBTYPE_PULSAR_C0_IRQ_MAIN2MCU_PLS | TISCI_DEV_MAIN2MCU_PLS_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
RESASG_TYPE_PULSAR_C1_IRQ | RESASG_SUBTYPE_PULSAR_C1_IRQ_MCU_NAV | TISCI_DEV_MCU_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
RESASG_SUBTYPE_PULSAR_C1_IRQ_WKUP_GPIO | TISCI_DEV_WKUP_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
RESASG_SUBTYPE_PULSAR_C1_IRQ_MAIN2MCU_LVL | TISCI_DEV_MAIN2MCU_LVL_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
RESASG_SUBTYPE_PULSAR_C1_IRQ_MAIN2MCU_PLS | TISCI_DEV_MAIN2MCU_PLS_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
RESASG_TYPE_ICSSG0_IRQ | RESASG_SUBTYPE_ICSSG0_IRQ_MAIN_NAV | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
RESASG_SUBTYPE_ICSSG0_IRQ_MAIN_GPIO | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
RESASG_TYPE_ICSSG1_IRQ | RESASG_SUBTYPE_ICSSG1_IRQ_MAIN_NAV | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
RESASG_SUBTYPE_ICSSG1_IRQ_MAIN_GPIO | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
RESASG_TYPE_ICSSG2_IRQ | RESASG_SUBTYPE_ICSSG1_IRQ_MAIN_NAV | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
RESASG_SUBTYPE_ICSSG1_IRQ_MAIN_GPIO | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
2.7.3.7.2. AM65X SR2 Sciclient Interrupt Resource Type Migration Table¶
Old Resource Type | Old Resource Subtype | New Resource Type | New Resource Subtype |
---|---|---|---|
AM6_DEV_MCU_CPSW0 | TISCI_RESASG_SUBTYPE_MCU_CPSW0_CPTS_HW3_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_MCU_CPSW0_CPTS_HW4_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
AM6_DEV_WKUP_DMSC0_CORTEX_M3_0 | TISCI_RESASG_SUBTYPE_WKUP_DMSC0_CORTEX_M3_0_NVIC_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 | TISCI_DEV_WKUP_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
AM6_DEV_ESM0 | TISCI_RESASG_SUBTYPE_ESM0_ESM_PLS_EVENT0_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_ESM0_ESM_PLS_EVENT1_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_ESM0_ESM_PLS_EVENT2_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
AM6_DEV_WKUP_ESM0 | TISCI_RESASG_SUBTYPE_WKUP_ESM0_ESM_PLS_EVENT0_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 | TISCI_DEV_WKUP_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_WKUP_ESM0_ESM_PLS_EVENT1_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 | TISCI_DEV_WKUP_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_WKUP_ESM0_ESM_PLS_EVENT2_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 | TISCI_DEV_WKUP_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
AM6_DEV_GIC0 | TISCI_RESASG_SUBTYPE_GIC0_SPI_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_GIC0_SPI_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_GIC0_SPI_IRQ_GROUP1_FROM_NAVSS0_INTR_ROUTER_0 | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_GIC0_SPI_IRQ_GROUP0_FROM_CMPEVENT_INTRTR0 | TISCI_DEV_CMPEVENT_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_GIC0_SPI_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 | TISCI_DEV_WKUP_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
AM6_DEV_PRU_ICSSG0 | TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_EDC0_LATCH0_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_EDC0_LATCH1_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_EDC1_LATCH0_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_EDC1_LATCH1_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_IEP0_CAP_INTR_REQ_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_IEP1_CAP_INTR_REQ_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_SLV_INTR_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_SLV_INTR_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
AM6_DEV_PRU_ICSSG1 | TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_EDC0_LATCH0_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_EDC0_LATCH1_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_EDC1_LATCH0_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_EDC1_LATCH1_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_IEP0_CAP_INTR_REQ_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_IEP1_CAP_INTR_REQ_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_SLV_INTR_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_SLV_INTR_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
AM6_DEV_PRU_ICSSG2 | TISCI_RESASG_SUBTYPE_PRU_ICSSG2_PR1_EDC0_LATCH0_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_PRU_ICSSG2_PR1_EDC0_LATCH1_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG2_PR1_EDC1_LATCH0_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG2_PR1_EDC1_LATCH1_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG2_PR1_IEP0_CAP_INTR_REQ_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG2_PR1_IEP1_CAP_INTR_REQ_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG2_PR1_SLV_INTR_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG2_PR1_SLV_INTR_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
AM6_DEV_NAVSS0 | TISCI_RESASG_SUBTYPE_NAVSS0_CPTS0_HW1_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_NAVSS0_CPTS0_HW2_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_NAVSS0_CPTS0_HW3_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_NAVSS0_CPTS0_HW4_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_NAVSS0_CPTS0_HW5_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_NAVSS0_CPTS0_HW6_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_NAVSS0_CPTS0_HW7_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_NAVSS0_CPTS0_HW8_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
AM6_DEV_PCIE0 | TISCI_RESASG_SUBTYPE_PCIE0_PCIE_CPTS_HW2_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
AM6_DEV_PCIE1 | TISCI_RESASG_SUBTYPE_PCIE1_PCIE_CPTS_HW2_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
AM6_DEV_PDMA1 | TISCI_RESASG_SUBTYPE_PDMA1_LEVENT_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_PDMA1_LEVENT_IN_IRQ_GROUP0_FROM_CMPEVENT_INTRTR0 | TISCI_DEV_CMPEVENT_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
AM6_DEV_MCU_ARMSS0_CPU0 | TISCI_RESASG_SUBTYPE_MCU_ARMSS0_CPU0_INTR_IRQ_GROUP0_FROM_MCU_NAVSS0_INTR_ROUTER_0 | TISCI_DEV_MCU_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_MCU_ARMSS0_CPU0_INTR_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 | TISCI_DEV_WKUP_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_MCU_ARMSS0_CPU0_INTR_IRQ_GROUP0_FROM_MAIN2MCU_LVL_INTRTR0 | TISCI_DEV_MAIN2MCU_LVL_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_MCU_ARMSS0_CPU0_INTR_IRQ_GROUP0_FROM_MAIN2MCU_PLS_INTRTR0 | TISCI_DEV_MAIN2MCU_PLS_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
AM6_DEV_MCU_ARMSS0_CPU1 | TISCI_RESASG_SUBTYPE_MCU_ARMSS0_CPU1_INTR_IRQ_GROUP0_FROM_MCU_NAVSS0_INTR_ROUTER_0 | TISCI_DEV_MCU_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_MCU_ARMSS0_CPU1_INTR_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 | TISCI_DEV_WKUP_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_MCU_ARMSS0_CPU1_INTR_IRQ_GROUP0_FROM_MAIN2MCU_LVL_INTRTR0 | TISCI_DEV_MAIN2MCU_LVL_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_MCU_ARMSS0_CPU1_INTR_IRQ_GROUP0_FROM_MAIN2MCU_PLS_INTRTR0 | TISCI_DEV_MAIN2MCU_PLS_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
2.7.3.7.3. J721E Sciclient Interrupt Resource Type Migration Table¶
Old Resource Type | Old Resource Subtype | New Resource Type | New Resource Subtype |
---|---|---|---|
TISCI_DEV_COMPUTE_CLUSTER0_CLEC | TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_CLEC_SOC_EVENTS_IN_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_CLEC_SOC_EVENTS_IN_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_CLEC_SOC_EVENTS_IN_IRQ_GROUP1_FROM_NAVSS0_INTR_ROUTER_0 | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_CLEC_SOC_EVENTS_IN_IRQ_GROUP0_FROM_CMPEVENT_INTRTR0 | TISCI_DEV_CMPEVENT_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_CLEC_SOC_EVENTS_IN_IRQ_GROUP2_FROM_NAVSS0_INTR_ROUTER_0 | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_CLEC_SOC_EVENTS_IN_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 | TISCI_DEV_WKUP_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_DEV_COMPUTE_CLUSTER0_GIC500SS | TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_GIC500SS_SPI_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_GIC500SS_SPI_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_GIC500SS_SPI_IRQ_GROUP1_FROM_NAVSS0_INTR_ROUTER_0 | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_GIC500SS_SPI_IRQ_GROUP0_FROM_CMPEVENT_INTRTR0 | TISCI_DEV_CMPEVENT_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_GIC500SS_SPI_IRQ_GROUP2_FROM_NAVSS0_INTR_ROUTER_0 | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_GIC500SS_SPI_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 | TISCI_DEV_WKUP_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_DEV_MCU_CPSW0 | TISCI_RESASG_SUBTYPE_MCU_CPSW0_CPTS_HW3_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_MCU_CPSW0_CPTS_HW4_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_DEV_CPSW0 | TISCI_RESASG_SUBTYPE_CPSW0_CPTS_HW1_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_CPSW0_CPTS_HW2_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_CPSW0_CPTS_HW3_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_CPSW0_CPTS_HW4_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_CPSW0_CPTS_HW5_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_CPSW0_CPTS_HW6_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_CPSW0_CPTS_HW7_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_CPSW0_CPTS_HW8_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_DEV_ESM0 | TISCI_RESASG_SUBTYPE_ESM0_ESM_PLS_EVENT0_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_ESM0_ESM_PLS_EVENT1_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_ESM0_ESM_PLS_EVENT2_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_DEV_WKUP_ESM0 | TISCI_RESASG_SUBTYPE_WKUP_ESM0_ESM_PLS_EVENT0_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 | TISCI_DEV_WKUP_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_WKUP_ESM0_ESM_PLS_EVENT1_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 | TISCI_DEV_WKUP_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_WKUP_ESM0_ESM_PLS_EVENT2_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 | TISCI_DEV_WKUP_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_DEV_PRU_ICSSG0 | TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_EDC0_LATCH0_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_EDC0_LATCH1_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_EDC1_LATCH0_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_EDC1_LATCH1_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_IEP0_CAP_INTR_REQ_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_IEP1_CAP_INTR_REQ_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_SLV_INTR_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_DEV_PRU_ICSSG1 | TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_EDC0_LATCH0_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_EDC0_LATCH1_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_EDC1_LATCH0_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_EDC1_LATCH1_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_IEP0_CAP_INTR_REQ_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_IEP1_CAP_INTR_REQ_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_SLV_INTR_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_DEV_C66SS0_CORE0 | TISCI_RESASG_SUBTYPE_C66SS0_CORE0_C66_EVENT_IN_SYNC_IRQ_GROUP0_FROM_C66SS0_INTROUTER0 | TISCI_DEV_C66SS0_INTROUTER0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_C66SS0_CORE0_C66_EVENT_IN_SYNC_IRQ_GROUP1_FROM_C66SS0_INTROUTER0 | TISCI_DEV_C66SS0_INTROUTER0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_C66SS0_CORE0_C66_EVENT_IN_SYNC_IRQ_GROUP2_FROM_C66SS0_INTROUTER0 | TISCI_DEV_C66SS0_INTROUTER0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_C66SS0_CORE0_C66_EVENT_IN_SYNC_IRQ_GROUP3_FROM_C66SS0_INTROUTER0 | TISCI_DEV_C66SS0_INTROUTER0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_C66SS0_CORE0_C66_EVENT_IN_SYNC_IRQ_GROUP4_FROM_C66SS0_INTROUTER0 | TISCI_DEV_C66SS0_INTROUTER0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_DEV_C66SS1_CORE0 | TISCI_RESASG_SUBTYPE_C66SS1_CORE0_C66_EVENT_IN_SYNC_IRQ_GROUP0_FROM_C66SS1_INTROUTER0 | TISCI_DEV_C66SS1_INTROUTER0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_C66SS1_CORE0_C66_EVENT_IN_SYNC_IRQ_GROUP1_FROM_C66SS1_INTROUTER0 | TISCI_DEV_C66SS1_INTROUTER0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_C66SS1_CORE0_C66_EVENT_IN_SYNC_IRQ_GROUP2_FROM_C66SS1_INTROUTER0 | TISCI_DEV_C66SS1_INTROUTER0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_C66SS1_CORE0_C66_EVENT_IN_SYNC_IRQ_GROUP3_FROM_C66SS1_INTROUTER0 | TISCI_DEV_C66SS1_INTROUTER0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_C66SS1_CORE0_C66_EVENT_IN_SYNC_IRQ_GROUP4_FROM_C66SS1_INTROUTER0 | TISCI_DEV_C66SS1_INTROUTER0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_DEV_NAVSS512L_MAIN_0 | TISCI_RESASG_SUBTYPE_NAVSS512L_MAIN_0_CPTS0_HW1_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_NAVSS512L_MAIN_0_CPTS0_HW2_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_NAVSS512L_MAIN_0_CPTS0_HW3_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_NAVSS512L_MAIN_0_CPTS0_HW4_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_NAVSS512L_MAIN_0_CPTS0_HW5_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_NAVSS512L_MAIN_0_CPTS0_HW6_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_NAVSS512L_MAIN_0_CPTS0_HW7_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_NAVSS512L_MAIN_0_CPTS0_HW8_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_DEV_NAVSS0_UDMASS_INTAGGR_0 | TISCI_RESASG_SUBTYPE_NAVSS0_UDMASS_INTAGGR_0_INTAGGR_LEVI_PEND_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_NAVSS0_UDMASS_INTAGGR_0_INTAGGR_LEVI_PEND_IRQ_GROUP0_FROM_CMPEVENT_INTRTR0 | TISCI_DEV_CMPEVENT_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_NAVSS0_UDMASS_INTAGGR_0_INTAGGR_LEVI_PEND_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_DEV_MCU_NAVSS0_INTAGGR_0 | TISCI_RESASG_SUBTYPE_MCU_NAVSS0_INTAGGR_0_INTAGGR_LEVI_PEND_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 | TISCI_DEV_WKUP_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_DEV_PCIE0 | TISCI_RESASG_SUBTYPE_PCIE0_PCIE_CPTS_HW2_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_DEV_PCIE1 | TISCI_RESASG_SUBTYPE_PCIE1_PCIE_CPTS_HW2_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_DEV_PCIE2 | TISCI_RESASG_SUBTYPE_PCIE2_PCIE_CPTS_HW2_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_DEV_PCIE3 | TISCI_RESASG_SUBTYPE_PCIE3_PCIE_CPTS_HW2_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 | TISCI_DEV_TIMESYNC_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_DEV_R5FSS0_CORE0 | TISCI_RESASG_SUBTYPE_R5FSS0_CORE0_INTR_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_R5FSS0_CORE0_INTR_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_R5FSS0_CORE0_INTR_IRQ_GROUP0_FROM_R5FSS0_INTROUTER0 | TISCI_DEV_R5FSS0_INTROUTER0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_DEV_R5FSS0_CORE1 | TISCI_RESASG_SUBTYPE_R5FSS0_CORE1_INTR_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_R5FSS0_CORE1_INTR_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_R5FSS0_CORE1_INTR_IRQ_GROUP0_FROM_R5FSS0_INTROUTER0 | TISCI_DEV_R5FSS0_INTROUTER0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_DEV_R5FSS1_CORE0 | TISCI_RESASG_SUBTYPE_R5FSS1_CORE0_INTR_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_R5FSS1_CORE0_INTR_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_R5FSS1_CORE0_INTR_IRQ_GROUP0_FROM_R5FSS1_INTROUTER0 | TISCI_DEV_R5FSS1_INTROUTER0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_DEV_R5FSS1_CORE1 | TISCI_RESASG_SUBTYPE_R5FSS1_CORE1_INTR_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 | TISCI_DEV_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_R5FSS1_CORE1_INTR_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_R5FSS1_CORE1_INTR_IRQ_GROUP0_FROM_R5FSS1_INTROUTER0 | TISCI_DEV_R5FSS1_INTROUTER0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_DEV_MCU_R5FSS0_CORE0 | TISCI_RESASG_SUBTYPE_MCU_R5FSS0_CORE0_INTR_IRQ_GROUP0_FROM_MCU_NAVSS0_INTR_ROUTER_0 | TISCI_DEV_MAIN2MCU_LVL_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_MCU_R5FSS0_CORE0_INTR_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 | TISCI_DEV_WKUP_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_MCU_R5FSS0_CORE0_INTR_IRQ_GROUP0_FROM_MAIN2MCU_LVL_INTRTR0 | TISCI_DEV_MAIN2MCU_LVL_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_MCU_R5FSS0_CORE0_INTR_IRQ_GROUP0_FROM_MAIN2MCU_PLS_INTRTR0 | TISCI_DEV_MAIN2MCU_PLS_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_MCU_R5FSS0_CORE0_INTR_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_DEV_MCU_R5FSS0_CORE1 | TISCI_RESASG_SUBTYPE_MCU_R5FSS0_CORE1_INTR_IRQ_GROUP0_FROM_MCU_NAVSS0_INTR_ROUTER_0 | TISCI_DEV_MCU_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
TISCI_RESASG_SUBTYPE_MCU_R5FSS0_CORE1_INTR_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 | TISCI_DEV_WKUP_GPIOMUX_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_MCU_R5FSS0_CORE1_INTR_IRQ_GROUP0_FROM_MAIN2MCU_LVL_INTRTR0 | TISCI_DEV_MAIN2MCU_LVL_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_MCU_R5FSS0_CORE1_INTR_IRQ_GROUP0_FROM_MAIN2MCU_PLS_INTRTR0 | TISCI_DEV_MAIN2MCU_PLS_INTRTR0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT | |
TISCI_RESASG_SUBTYPE_MCU_R5FSS0_CORE1_INTR_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 | TISCI_DEV_NAVSS0_INTR_ROUTER_0 | TISCI_RESASG_SUBTYPE_IR_OUTPUT |
2.7.4. Device Support¶
- AM65xx EVM, AM65xx IDK, AM65xx-HS EVM (BOARD=am65xx_evm, am65xx_idk)
- J721E EVM, J721E-HS EVM (BOARD=j721e_evm)
2.7.5. Validation Information¶
This release is validated on above devices for the applicable components. For details on the validated examples refer to the platform specific test report present in PDK_INSTALL_DIR/docs/test_report folder.
2.7.6. Tool Chain Information¶
Refer to SDK level documentation for Tool Chain and dependent component version used to validate this release.
2.7.7. Fixed Issues¶
ID | Head Line | Module | Affected Versions | Affected Platforms |
---|---|---|---|---|
PDK-5764 | R5F MPU configuration for ATCM and BTCM is wrong in r5_mpu.xs for J721E and J7200 | BUILD | 06.02.00 | j721e-evm |
PDK-5759 | Incorrect status for memory attributes in r5_mpu.xs for j721e and j7200 for DDR | BUILD | 06.02.00 | j721e-evm |
PRSDK-7244 | CSL Serdes configuration for PCIE Gen2 is unreliable | CSL | 06.01.00 | am654x-evm, am654x-idk |
PRSDK-7754 | LPDDR CSL-FL: Missing API to read and write thermal monitor | CSL | 06.02.00 | j721e-evm |
PDK-4959 | [Boot App]Compilation Error During Boot App Build | CSL | 06.02.00 | j721e-evm |
PDK-5070 | Latest Uniflash documentation is not included in the release | COMMON | 06.02.00 | j721e-evm |
PDK-6378 | [DSS]DSS sample application crashes with DMSC flow | DSS | 06.02.00 | am654x-evm |
PRSDK-7735 | am65xx: Need to optimize time it takes to polll for packets from udma rings on R5 | EMAC | 06.02.00 | am654x-idk |
PRSDK-8081 | GPIO instance is hardcoded in GPIO driver | GPIO | 06.02.00 | j721e-evm |
PRSDK-7933 | Mailbox irq does not work on mcu1_1 using dynamic allocation | IPC | 06.01.00 | j721e-evm |
PRSDK-8481 | OSAL: Timer API wrongly uses HWIP clear and disable interrupts, instead of OSAL clear and disable APIs | OSAL | 06.03.00 | am654x-evm, am654x-hsevm, am654x-idk, j721e-evm |
PDK-5588 | OSAL API TimerP_Params_init() initializes the Timer with wrong default clock (25MHz) | OSAL | 06.02.00 | j721e-evm |
PRSDK-8426 | OSAL: SemaphoreP_postfromISR() API does not work for baremetal | OSAL | 06.02.00 | j721e-evm |
PDK-6685 | Timer osal - noos - Uninitialized variable | OSAL | 06.02.00 | j721e-evm |
PRSDK-5415 | RTOS: K3: fix issue in OSPI INDAC mode with interrupt enabled for J7 | OSPI | 05.02.00 | j721e-evm |
PRSDK-8301 | OSPI configured in SDR mode is not stable for SBL image copies | OSPI | 06.02.00 | j721e-evm |
PDK-5600 | OSPI FLash timing optimization | OSPI | 06.02.00 | j721e-evm |
PDK-6294 | SA: AM65x: Unit test aborts due to memory allocation failure | SA2UL | 06.02.00 | am654x-evm |
PRSDK-8302 | Board config for SBL is not setting proper value for GTC clock in MAIN domain | SBL | 06.02.00 | j721e-evm |
PDK-5733 | [Boot] Certificate Parsing for X509 SBL is not fool proof | SBL | 06.02.00 | j721e-evm |
PDK-5645 | SBL configures MCU DMTimer0 for 250MHz while BIOS Timer.xs expects it to be at 19.2MHz | SBL | 06.02.00 | j721e-evm |
PDK-5574 | ipc: messages coming twice unexpectedly | IPC | 06.02.00 | j721e-evm |
PDK-5573 | ipc: heapAlloc is not returning NULL when allocation fails | IPC | 06.02.00 | j721e-evm |
PDK-5572 | ipc: echo tests: Linux vrings not properly configured for non-cached for some cores | IPC | 06.02.00 | am654x-evm, j721e-evm |
PDK-5146 | IPC: tests: Board_init with pinmux config is conflicting with other test firmware | IPC | 06.02.00 | j721e-evm |
PDK-5261 | [SCICLIENT] Sciclient PM functions send NULL request payloads | SCICLIENT | 06.02.00 | am654x-evm |
PDK-5033 | [SCICLIENT] Alignment mismatches in C66x causes the response to not be captured correctly | SCICLIENT | 06.02.00 | j721e-evm |
PDK-4963 | {SCICLIENT] Build fails intermittendly | SCICLIENT | 06.02.00 | j721e-evm |
PDK-4948 | Launch.js file fails when running OSPI boot mode | SCICLIENT | 06.02.00 | j721e-evm |
PDK-4994 | [UDMA] Proxy access fails when using CPSW LLD from QNX | UDMA | 06.02.00 | am654x-evm, j721e-evm |
PDK-6522 | udma - Ring occupancy becoming negative | UDMA | 06.02.00 | j721e-evm |
PDK-5221 | Spurious Interrupts observed for MSC & other modules in VPAC | VHWA | 06.01.00 | j721e-evm |
PDK-5804 | VPAC VISS H3A driver does not check for invalid parameters | VHWA | 06.02.00 | j721e-evm |
PDK-6701 | [VISS]:Edge Enhancer does not work for YUV422 output | VHWA | 06.02.00 | j721e-evm |
PRSDK-7492 | Uniflash requires extra Serial-Cable Unplug/Re-plug step during operation | UNIFLASH | 06.01.00 | am654x-evm, am654x-hsevm, am654x-idk |
PDK-5262 | [BOARD LIB]UB960 pattern generation API programs UB960 in case of error | BOARD | 06.02.00 | j721e-evm |
PDK-5147 | [Board Lib]Board lib does not support more the 1 active I2C instances | BOARD | 06.02.00 | j721e-evm |
PDK-5016 | [j721e board] Serdes config function uses serdesInstance value for phyInstance | BOARD | 06.02.00 | j721e-evm |
PRSDK-7908 | R5 Board Diagnostics Apploader crashes | BOARD DIAG | 06.02.00 | am654x-evm, am654x-hsevm, am654x-idk, j721e-evm |
PRSDK-7889 | Audio DC diagnostic test failure | BOARD DIAG | 06.01.00 | j721e-evm |
PRSDK-7176 | AM65x R5 diagnostic tests are hanging while running from diag framework | BOARD DIAG | 06.01.00 | am654x-evm, am654x-idk |
PRSDK-4661 | AM65x: Board diagnostics LCD touchscreen test reports incorrect number of touch events | BOARD DIAG | 05.01.00 | am654x-evm, am654x-hsevm, am654x-idk |
ETHFW-1570 | CPSW DMA - Ring monitor not allocated even though enabled by an application | CPSW | 06.02.00 | j721e-evm |
ETHFW-1564 | ETHFW-1564 - Examples - Sciclient_rmIrqSet fails for mcu2_1 examples due IR conflict | CPSW | 06.02.00 | j721e-evm |
ETHFW-1496 | CPSW PHY: dp83867: Robust auto-mdix is disabled for non-loopback mode | CPSW | 06.02.00 | j721e-evm |
ETHFW-1497 | CPSW - MAC reset is not released in SGMII 100/10 Mbps mode | CPSW | 06.02.00 | j721e-evm |
2.7.8. Known Issues¶
ID | Head Line | Module | Reported in Release | Affected Platforms | Impact | Workaround in this release |
---|---|---|---|---|---|---|
PDK-6549 | MCU2 core diagnostic tests not running through sbl | BOARD | 07.00.00 | j721e_evm | None | Use CCS/JTAG to run the tests |
PDK-6548 | Display port (eDP) diagnostic test failure | BOARD | 07.00.00 | j721e_evm | None | Use display sample application |
PDK-6707 | PCIe diagnostic test failure | BOARD | 07.00.00 | am65xx_evm, am65xx_idk | None | Use PCIe driver sample application |
PRSDK-7891 | CPSW RGMII diagnostic test failure | BOARD | 06.01.00 | j721e-evm | None | None |
PRSDK-8607 | Board_init(SBL_PLL_INIT) is configuring PLL directly without going through SYSFW. | BOARD | 06.03.00 | am654x-idk, am64x-evm | None | Comment below lines of code from Board_PLLInitAll() (pdk/packages/ti/board/src/evmKeystone3) Board_PLLConfig(&pllcConfigs[CSL_PER0_PLL]); Board_PLLConfig(&pllcConfigs[CSL_MCU_PLL]); Board_PLLConfig(&pllcConfigs[CSL_CPSW_PLL]); |
PDK-6762 | CSL: UART test fails for MCU 1_0 | CSL | 07.00.00 | am65xx_evm, j721e_evm | Low. There are other CSL examples that output to UART without any issue. Additionally, this test works fine for MPU1_0. Suspect this is a CSL example application. | Use UART driver in baremetal mode |
PDK-6800 | AM65: Watchdog timer diagnostic test fails | DIAG | 07.00.00 | am65xx_evm | The watchdog timer has been tested successfully on AM65 using CSL test. Suspect the diagnostics test may have a timing issue | None |
PDK-5224 | Active DP -> HDMI adapter doesn’t work | DSS | 00.09.01 | j721e_evm | DP to HDMI adapter for display cannot be used. | None |
PDK-5040 | Display stops working if two pipelines are started back to back | DSS | 06.02.00 | j721e_evm | None, if the workaround is in place. | Wait for a frame to go out from a pipeline before starting the next one |
PDK-6734 | am65xx: emac: Driver updates to support wire clock feature in TX CFG | EMAC | 07.00.00 | am65xx_idk | There will be jitter in the inter arrival packet gap when transmitting packets at a high data rate | None |
PRSDK-5022 | am65xx: Running emac unit test on R5 core from ddrless SBL at times does not complete execution | EMAC | 05.02.00 | am654x-evm, am654x-idk | Running emac unit test which does not access DDR from SBL does not finish execution, this unit test only added to run on R5 core | None |
PDK-6791 | i2c eeprom smp testapp load fails | I2C | 07.00.00 | am65xx_evm | The issue is most likely a application configuration or test setup issue as other SMP applications are working fine | None. Use non-SMP mode |
PDK-6742 | McASP regression test app some tests are failing | McASP | 07.00.00 | am65xx_evm | The issue is most likely a application configuration | None |
PDK-6743 | McASP SMP tests fails | McASP | 07.00.00 | am65xx_evm, j721e_evm | The issue is most likely a application configuration or test setup issue as other SMP applications are working fine | None. Use non-SMP mode |
PRSDK-5074 | McASP driver hangs with small buffer size | McASP | 05.01.00 | am654x-evm, j721e-evm | None | Use packet size 32 samples or greater |
PDK-6649 | Timer osal - noos - Timer delete doesn’t “free” timer | OSAL | 06.02.00 | j721e_evm | Resource leak if create/delete called in a loop. But typically this is not done for Timer. | Use the same timer in the application without create/deleting multiple times |
PDK-6534 | Timer osal - noos - Timer should be reset first before registering interrupts | OSAL | 06.02.00 | j721e_evm | None if the workaround is in place | Reset the timer before using |
PDK-6758 | pcie qos examples fails for 2 lane configuration | PCIE | 07.00.00 | am65xx_idk | None | None |
PRSDK-8036 | PCIE-0: Intermittent failures during Gen 3 mode on AM65x PG2.0 | PCIE | 06.02.00 | am654x-evm, am654x-idk | None | None |
PDK-6415 | PMIC: Need to support asynchronous interrupts | PMIC | 07.00.00 | j721e_evm | Asynchronous Interrupt feature is not supported | None |
PDK-6440 | PMIC: SBL test for GPIO Interrupts on Pins 3 and 4 are causing Hang on J721 EVM | PMIC | 07.00.00 | j721e_evm | GPIO Pin 3 and 4 is not supported while testing with SBL | GPIO Pin 3 and 4 functionalities can be tested using CCS |
PDK-6439 | PMIC: GPIO Interrupt tests on Pin 7, 9 and 11 are failing | PMIC | 07.00.00 | j721e_evm | GPIO Interrupt feature for Pin 7, 9 11 is not supported | GPIO Interrupt feature for other Pins except 7, 9 11 is supported |
PDK-6757 | PMIC: SBL test for RTC unit tests results in hang for mcu1_1 core | PMIC | 07.00.00 | j721e_evm | PMIC RTC Test application fails while testing with SBL | PMIC RTC Test application is supported on muc1_1 core using CCS |
PRSDK-6382 | SBL: R5F: Core 1 boot is not working with unsigned binary with ipc images | SBL | 06.01.00 | am654x-evm | None | None |
PRSDK-5448 | SBL boot from MMCSD fails intermittently | SBL | 05.02.00 | am654x-evm, am654x-idk | None | The workaround involves configuring the MMCSD driver in DS mode instead of the default HS mode. This can be done by making the below change in SBL’s mmcsd config file pdk/packages/ti/boot/sbl/src/mmcsd/sbl_mmcsd.c#n232 Before calling the function MMCSD_socSetInitCfg(), insert the below line hwAttrsConfig.supportedModes = MMCSD_SUPPORT_SD_DS; Rebuild the MMCSD SBL image (sbl_mmcsd_img) cd pdk_<ver>/packages/ti/build make sbl_mmcsd_img_clean BOARD=<board> CORE=mcu1_0 make sbl_mmcsd_img BOARD=<board> CORE=mcu1_0 Use the sbl_mmcsd_img built above |
PRSDK-5626 | OSPI Read using UDMA fails on AM65x HS devices. | SBL | 05.03.00 | am654x-hsevm | None | Non-DMA mode could be used for the read operation |
PDK-6789 | MCU/Main NAVSS UDMA memcpy from L2SRAM fails | UDMA | 07.00.00 | j721e_evm | Transfer works fine when source buffer, destination buffer and TRPD buffers are in L2SRAM. The issue happens only when the ring memory is in L2SRAM location | Use ring memory from non-L2SRAM location |
PRSDK-5989 | USB Host MSC test hangs in SMP mode on AM65xx IDK board | USB | 06.00.00 | am654x-idk | None | None. Use non-SMP mode |
PDK-5228 | Output mismatch when each region requiring 3 TRs | VHWA | 01.00.00 | j721e_evm | In multi-region mode with more then 3 TR per region can’t be used | In multi-region mode for each region less than 3 TR should be used |
PDK-5226 | DOF generated wrong output with SOF if pixel in all row are not enabled | VHWA | 01.00.00, 00.09.01 | j721e_evm | When using the SOF if the Paxel rows without any pixel enabled is not in consecutive pair with lead to lead to output mismatch | This issue is due to shift in flowvector out buffer. While generating the SOF binary map make sure that Paxel rows without any pixel enabled should be in consecutive pair |
PDK-5217 | VPAC VISS driver doesn’t support several valid mux combinations for outputs | VHWA | 01.00.00, 00.09.01 | j721e_evm | VISS output with Chroma only and one of the RGB component enabled may not work | Enable YUV420 instead of Chroma only while using RGB component |
2.7.9. Limitations¶
- Active DP -> HDMI adapter doesn’t work. As a workaround use the display that supports Active DP