PDK API Guide for J721E
|
DMSC controls the power management of the device, hence is responsible for bringing the device out of reset, enforce clock and reset rules. DMSC power management functions are critical to bring device to low power modes, for example DeepSleep, and sense wake-up events to bring device back online to active state.
Files | |
file | sciclient_pm.h |
This file contains the definition of all the message IDs, message formats to be able to interact with the System Controller firmware for power management. | |
Functions | |
int32_t | Sciclient_pmSetModuleState (uint32_t moduleId, uint32_t state, uint32_t reqFlag, uint32_t timeout) |
Message to set the hardware block/module state This is used to request or release a device. For example: When the device is requested for operation, state is set to MSG_DEVICE_SW_STATE_ON. When the usage of the device is complete and released, the same request with state set as MSG_DEVICE_SW_STATE_AUTO_OFF is invoked. Based on exclusive access request, multiple processing entities can share a specific hardware block, however, this must be carefully used keeping the full system view in mind. More... | |
int32_t | Sciclient_pmGetModuleState (uint32_t moduleId, uint32_t *moduleState, uint32_t *resetState, uint32_t *contextLossState, uint32_t timeout) |
Message to get the hardware block/Module state. This request does not require the processing entity to have control of the device via a set device state request. More... | |
int32_t | Sciclient_pmSetModuleRst (uint32_t moduleId, uint32_t resetBit, uint32_t timeout) |
Set the device reset state. This is used to set or release various resets of the hardware block/module. More... | |
int32_t | Sciclient_pmSetModuleRst_flags (uint32_t moduleId, uint32_t resetBit, uint32_t reqFlag, uint32_t timeout) |
Set the device reset state, allowing for user to set reqFlags This is used to set or release various resets of the hardware block/module. More... | |
int32_t | Sciclient_pmModuleClkRequest (uint32_t moduleId, uint32_t clockId, uint32_t state, uint32_t additionalFlag, uint32_t timeout) |
Message to set the clock state: This requests for finer control of hardware device's clocks. This allows for configuration for hardware blocks that require customization of the specific input clocks. NOTE: each of the clock IDs are relative to the hardware block. More... | |
int32_t | Sciclient_pmModuleGetClkStatus (uint32_t moduleId, uint32_t clockId, uint32_t *state, uint32_t timeout) |
Message to get the clock state to or from a hardware block. More... | |
int32_t | Sciclient_pmSetModuleClkParent (uint32_t moduleId, uint32_t clockId, uint32_t parent, uint32_t timeout) |
Message to Set Clock Parent: This message allows SoC specific customization for setting up a specific clock parent ID for the various clock input options for a hardware block's clock. This is rarely used customization that may be required based on the usecase of the system where the reset input clock option may not suffice for the usecase attempted. More... | |
int32_t | Sciclient_pmGetModuleClkParent (uint32_t moduleId, uint32_t clockId, uint32_t *parent, uint32_t timeout) |
Message to Get Clock Parent: Query the clock parent currently configured for a specific clock source of a hardware block This is typically used to confirm the current clock parent to ensure that the requisite usecase for the hardware block can be satisfied. More... | |
int32_t | Sciclient_pmGetModuleClkNumParent (uint32_t moduleId, uint32_t clockId, uint32_t *numParent, uint32_t timeout) |
Message to get the number of clock parents for a given module. This is typically used to get the max number of clock parent options available for a specific hardware block's clock. More... | |
int32_t | Sciclient_pmSetModuleClkFreq (uint32_t moduleId, uint32_t clockId, uint64_t freqHz, uint32_t additionalFlag, uint32_t timeout) |
Message to set the clock frequency. This is typically desired when the default frequency of the hardware block's clock is not appropriate for the usecase desired. NOTE: Normally clock frequency management is automatically done by TISCI entity. In case of specific requests, TISCI evaluates capability to achieve requested range and responds with success/failure message. This sets the desired frequency for a clock within an allowable range. This message will fail on an enabled clock unless MSG_FLAG_CLOCK_ALLOW_FREQ_CHANGE is set for the clock. Additionally, if other clocks have their frequency modified due to this message, they also must have the MSG_FLAG_CLOCK_ALLOW_FREQ_CHANGE or be disabled. More... | |
int32_t | Sciclient_pmSetModuleClkFreqRange (uint32_t moduleId, uint32_t clockId, uint64_t freqHz, uint64_t minFreqHz, uint64_t maxFreqHz, uint32_t additionalFlag, uint32_t timeout) |
Message to set the clock frequency. This is typically desired when the default frequency of the hardware block's clock is not appropriate for the usecase desired. NOTE: Normally clock frequency management is automatically done by TISCI entity. In case of specific requests, TISCI evaluates capability to achieve requested range and responds with success/failure message. This sets the desired frequency for a clock within an allowable range. This message will fail on an enabled clock unless MSG_FLAG_CLOCK_ALLOW_FREQ_CHANGE is set for the clock. Additionally, if other clocks have their frequency modified due to this message, they also must have the MSG_FLAG_CLOCK_ALLOW_FREQ_CHANGE or be disabled. More... | |
int32_t | Sciclient_pmQueryModuleClkFreq (uint32_t moduleId, uint32_t clockId, uint64_t reqFreqHz, uint64_t *respFreqHz, uint32_t timeout) |
Message to query the best clock frequency in the given range. This message does no real operation, instead, it requests the system control entity to respond with the best frequency that can match a frequency range provided. NOTE: This is a snapshot view. In a multi processing system, it is very well possible that another processing entity might change the configuration after one entity has queried for best match capability. Only a SET_CLOCK_FREQ will guarantee the frequency is configured. More... | |
int32_t | Sciclient_pmQueryModuleClkFreqRange (uint32_t moduleId, uint32_t clockId, uint64_t reqFreqHz, uint64_t minFreqHz, uint64_t maxFreqHz, uint64_t *respFreqHz, uint32_t timeout) |
Message to query the best clock frequency in the given range. This message does no real operation, instead, it requests the system control entity to respond with the best frequency that can match a frequency range provided. NOTE: This is a snapshot view. In a multi processing system, it is very well possible that another processing entity might change the configuration after one entity has queried for best match capability. Only a SET_CLOCK_FREQ will guarantee the frequency is configured. More... | |
int32_t | Sciclient_pmGetModuleClkFreq (uint32_t moduleId, uint32_t clockId, uint64_t *freqHz, uint32_t timeout) |
Message to Get Clock Frequency This is most used functionality and is meant for usage when the driver controlling the hardware block requires to know the input clock frequency for configuring internal dividers / multipliers as required. More... | |
int32_t | Sciclient_pmEnableWdt (uint32_t timeout) |
Enables the WDT controllers within the DMSC. More... | |
int32_t | Sciclient_pmDisableWakeup (uint32_t timeout) |
This message is part of the CPU Off sequence. The sequence is: More... | |
int32_t | Sciclient_pmGetWakeupReason (uint8_t mode[32], uint8_t reason[32], uint32_t *time_ms, uint32_t timeout) |
Request wakeup reason After a wakeup, the host can request the deepest sleep/idle mode reached and the reason for the wakeup. The API also returns the time spent in idle state. More... | |
int32_t | Sciclient_pmDevicePowerOff (uint32_t timeout) |
Some processors have a special sequence for powering off the core that provides notification to the PMMC when that sequence has completed. For processors without such a sequence, the goodbye message exists. The exact sequence involved in the goodbye message depends on the SoC. More... | |
int32_t | Sciclient_pmDeviceReset (uint32_t timeout) |
Objective: Trigger a SoC level reset Usage: Used to trigger a system level reset. NOTE: Depending on permissions configured for the SoC, not all processing entities may be permitted to request a SoC reset. When permitted, the request once processed will not return back to caller. More... | |
int32_t | Sciclient_pmDomainReset (domgrp_t domGrp, uint32_t timeout) |
Objective: Trigger a SoC level reset to parts of the SoC. More... | |
int32_t | Sciclient_pmIsModuleValid (uint32_t modId) |
This API would check if the given module Id is valid for the device. More... | |
Macros | |
#define | DOMGRP_00 ((0x01U) << 0U) |
#define | DOMGRP_01 ((0x01U) << 1U) |
#define | DOMGRP_02 ((0x01U) << 2U) |
#define | DOMGRP_03 ((0x01U) << 3U) |
#define | DOMGRP_04 ((0x01U) << 4U) |
#define | DOMGRP_05 ((0x01U) << 5U) |
#define | DOMGRP_06 ((0x01U) << 6U) |
#define DOMGRP_00 ((0x01U) << 0U) |
SoC defined domgrp 00
#define DOMGRP_01 ((0x01U) << 1U) |
SoC defined domgrp 01
#define DOMGRP_02 ((0x01U) << 2U) |
SoC defined domgrp 02
#define DOMGRP_03 ((0x01U) << 3U) |
SoC defined domgrp 03
#define DOMGRP_04 ((0x01U) << 4U) |
SoC defined domgrp 04
#define DOMGRP_05 ((0x01U) << 5U) |
SoC defined domgrp 05
#define DOMGRP_06 ((0x01U) << 6U) |
SoC defined domgrp 06
int32_t Sciclient_pmSetModuleState | ( | uint32_t | moduleId, |
uint32_t | state, | ||
uint32_t | reqFlag, | ||
uint32_t | timeout | ||
) |
Message to set the hardware block/module state This is used to request or release a device. For example: When the device is requested for operation, state is set to MSG_DEVICE_SW_STATE_ON. When the usage of the device is complete and released, the same request with state set as MSG_DEVICE_SW_STATE_AUTO_OFF is invoked. Based on exclusive access request, multiple processing entities can share a specific hardware block, however, this must be carefully used keeping the full system view in mind.
Message: TISCI_MSG_SET_DEVICE
Request: tisci_msg_set_device_req
Response: tisci_msg_set_device_resp
moduleId | Module for which the state should be set. Refer Sciclient_PmDeviceIds. |
state | Module State requested. |
reqFlag | Can be TISCI_MSG_FLAG_AOR/TISCI_MSG_FLAG_AOP ORRed |
with additional flag that can be set to alter the device state.
timeout | Gives a sense of how long to wait for the operation. Refer Sciclient_ServiceOperationTimeout. |
int32_t Sciclient_pmGetModuleState | ( | uint32_t | moduleId, |
uint32_t * | moduleState, | ||
uint32_t * | resetState, | ||
uint32_t * | contextLossState, | ||
uint32_t | timeout | ||
) |
Message to get the hardware block/Module state. This request does not require the processing entity to have control of the device via a set device state request.
Message: TISCI_MSG_GET_DEVICE
Request: tisci_msg_get_device_req
Response: tisci_msg_get_device_resp
moduleId | Module for which the state should be set. Refer Sciclient_PmDeviceIds. |
moduleState | Module State returned. |
resetState | Programmed state of the reset lines. |
contextLossState | Indicates how many times the device has lost context. A driver can use this monotonic counter to determine if the device has lost context since the last time this message was exchanged. |
timeout | Gives a sense of how long to wait for the operation. Refer Sciclient_ServiceOperationTimeout. |
int32_t Sciclient_pmSetModuleRst | ( | uint32_t | moduleId, |
uint32_t | resetBit, | ||
uint32_t | timeout | ||
) |
Set the device reset state. This is used to set or release various resets of the hardware block/module.
Message: TISCI_MSG_SET_DEVICE_RESETS
Request: tisci_msg_set_device_resets_req
Response: tisci_msg_set_device_resets_resp
moduleId | Module for which the state should be set. |
resetBit | Module Reset Bit to be set. 1 - Assert the reset 0 - Deassert the reset Note this convention is opposite of PSC MDCTL |
timeout | Gives a sense of how long to wait for the operation. Refer Sciclient_ServiceOperationTimeout. |
int32_t Sciclient_pmSetModuleRst_flags | ( | uint32_t | moduleId, |
uint32_t | resetBit, | ||
uint32_t | reqFlag, | ||
uint32_t | timeout | ||
) |
Set the device reset state, allowing for user to set reqFlags This is used to set or release various resets of the hardware block/module.
Message: TISCI_MSG_SET_DEVICE_RESETS
Request: tisci_msg_set_device_resets_req
Response: tisci_msg_set_device_resets_resp
moduleId | Module for which the state should be set. |
resetBit | Module Reset Bit to be set. 1 - Assert the reset 0 - Deassert the reset Note this convention is opposite of PSC MDCTL |
reqFlag | Can be TISCI_MSG_FLAG_AOR/TISCI_MSG_FLAG_AOP ORRed with additional flag that can be set to alter the device state. |
timeout | Gives a sense of how long to wait for the operation. Refer Sciclient_ServiceOperationTimeout. |
int32_t Sciclient_pmModuleClkRequest | ( | uint32_t | moduleId, |
uint32_t | clockId, | ||
uint32_t | state, | ||
uint32_t | additionalFlag, | ||
uint32_t | timeout | ||
) |
Message to set the clock state: This requests for finer control of hardware device's clocks. This allows for configuration for hardware blocks that require customization of the specific input clocks. NOTE: each of the clock IDs are relative to the hardware block.
Message: TISCI_MSG_SET_CLOCK
Request: tisci_msg_set_clock_req
Response: tisci_msg_set_clock_resp
moduleId | Module for which the state should be set. |
clockId | Clock Id for the module. |
state | Clock State requested. |
additionalFlag | Certain flags can also be set to alter the clock state. |
timeout | Gives a sense of how long to wait for the operation. |
int32_t Sciclient_pmModuleGetClkStatus | ( | uint32_t | moduleId, |
uint32_t | clockId, | ||
uint32_t * | state, | ||
uint32_t | timeout | ||
) |
Message to get the clock state to or from a hardware block.
Message: TISCI_MSG_GET_CLOCK
Request: tisci_msg_get_clock_req
Response: tisci_msg_get_clock_resp
moduleId | Module for which the state should be set. Refer Sciclient_PmDeviceIds. |
clockId | Clock Id for the module. Refer Sciclient_PmModuleClockIds. |
state | Clock State returned. |
timeout | Gives a sense of how long to wait for the operation. Refer Sciclient_ServiceOperationTimeout. |
int32_t Sciclient_pmSetModuleClkParent | ( | uint32_t | moduleId, |
uint32_t | clockId, | ||
uint32_t | parent, | ||
uint32_t | timeout | ||
) |
Message to Set Clock Parent: This message allows SoC specific customization for setting up a specific clock parent ID for the various clock input options for a hardware block's clock. This is rarely used customization that may be required based on the usecase of the system where the reset input clock option may not suffice for the usecase attempted.
Message: TISCI_MSG_SET_CLOCK_PARENT
Request: tisci_msg_set_clock_parent_req
Response: tisci_msg_set_clock_parent_resp
moduleId | Module for which the state should be set. Refer Sciclient_PmDeviceIds. |
clockId | Clock Id for the module. Refer Sciclient_PmModuleClockIds. |
parent | Parent Id for the clock. TODO: Find what this is. |
timeout | Gives a sense of how long to wait for the operation. Refer Sciclient_ServiceOperationTimeout. |
int32_t Sciclient_pmGetModuleClkParent | ( | uint32_t | moduleId, |
uint32_t | clockId, | ||
uint32_t * | parent, | ||
uint32_t | timeout | ||
) |
Message to Get Clock Parent: Query the clock parent currently configured for a specific clock source of a hardware block This is typically used to confirm the current clock parent to ensure that the requisite usecase for the hardware block can be satisfied.
Message: TISCI_MSG_GET_CLOCK_PARENT
Request: tisci_msg_get_clock_parent_req
Response: tisci_msg_get_clock_parent_resp
moduleId | Module for which the state should be set. Refer Sciclient_PmDeviceIds. |
clockId | Clock Id for the module. Refer Sciclient_PmModuleClockIds. |
parent | Returned Parent Id for the clock. TODO: Find what this is. |
timeout | Gives a sense of how long to wait for the operation. Refer Sciclient_ServiceOperationTimeout. |
int32_t Sciclient_pmGetModuleClkNumParent | ( | uint32_t | moduleId, |
uint32_t | clockId, | ||
uint32_t * | numParent, | ||
uint32_t | timeout | ||
) |
Message to get the number of clock parents for a given module. This is typically used to get the max number of clock parent options available for a specific hardware block's clock.
Message: TISCI_MSG_GET_NUM_CLOCK_PARENTS
Request: tisci_msg_get_num_clock_parents_req
Response: tisci_msg_get_num_clock_parents_resp
moduleId | Module for which the state should be set. Refer Sciclient_PmDeviceIds. |
clockId | Clock Id for the module. Refer Sciclient_PmModuleClockIds. |
numParent | Returned number of parents. |
timeout | Gives a sense of how long to wait for the operation. Refer Sciclient_ServiceOperationTimeout. |
int32_t Sciclient_pmSetModuleClkFreq | ( | uint32_t | moduleId, |
uint32_t | clockId, | ||
uint64_t | freqHz, | ||
uint32_t | additionalFlag, | ||
uint32_t | timeout | ||
) |
Message to set the clock frequency. This is typically desired when the default frequency of the hardware block's clock is not appropriate for the usecase desired. NOTE: Normally clock frequency management is automatically done by TISCI entity. In case of specific requests, TISCI evaluates capability to achieve requested range and responds with success/failure message. This sets the desired frequency for a clock within an allowable range. This message will fail on an enabled clock unless MSG_FLAG_CLOCK_ALLOW_FREQ_CHANGE is set for the clock. Additionally, if other clocks have their frequency modified due to this message, they also must have the MSG_FLAG_CLOCK_ALLOW_FREQ_CHANGE or be disabled.
Message: TISCI_MSG_SET_FREQ
Request: tisci_msg_set_freq_req
Response: tisci_msg_set_freq_resp
moduleId | Module for which the state should be set. Refer Sciclient_PmDeviceIds. |
clockId | Clock Id for the module. Refer Sciclient_PmModuleClockIds. |
freqHz | Frequency of the clock in Hertz. |
timeout | Gives a sense of how long to wait for the operation. Refer Sciclient_ServiceOperationTimeout. |
additionalFlag | Additional flags for the request. |
int32_t Sciclient_pmSetModuleClkFreqRange | ( | uint32_t | moduleId, |
uint32_t | clockId, | ||
uint64_t | freqHz, | ||
uint64_t | minFreqHz, | ||
uint64_t | maxFreqHz, | ||
uint32_t | additionalFlag, | ||
uint32_t | timeout | ||
) |
Message to set the clock frequency. This is typically desired when the default frequency of the hardware block's clock is not appropriate for the usecase desired. NOTE: Normally clock frequency management is automatically done by TISCI entity. In case of specific requests, TISCI evaluates capability to achieve requested range and responds with success/failure message. This sets the desired frequency for a clock within an allowable range. This message will fail on an enabled clock unless MSG_FLAG_CLOCK_ALLOW_FREQ_CHANGE is set for the clock. Additionally, if other clocks have their frequency modified due to this message, they also must have the MSG_FLAG_CLOCK_ALLOW_FREQ_CHANGE or be disabled.
Message: TISCI_MSG_SET_FREQ
Request: tisci_msg_set_freq_req
Response: tisci_msg_set_freq_resp
moduleId | Module for which the state should be set. Refer Sciclient_PmDeviceIds. |
clockId | Clock Id for the module. Refer Sciclient_PmModuleClockIds. |
freqHz | Frequency of the clock in Hertz. |
minFreqHz | Frequency of the clock in Hertz(Min Limit). |
maxFreqHz | Frequency of the clock in Hertz(Max Limit). |
timeout | Gives a sense of how long to wait for the operation. Refer Sciclient_ServiceOperationTimeout. |
additionalFlag | Additional flags for the request. |
int32_t Sciclient_pmQueryModuleClkFreq | ( | uint32_t | moduleId, |
uint32_t | clockId, | ||
uint64_t | reqFreqHz, | ||
uint64_t * | respFreqHz, | ||
uint32_t | timeout | ||
) |
Message to query the best clock frequency in the given range. This message does no real operation, instead, it requests the system control entity to respond with the best frequency that can match a frequency range provided. NOTE: This is a snapshot view. In a multi processing system, it is very well possible that another processing entity might change the configuration after one entity has queried for best match capability. Only a SET_CLOCK_FREQ will guarantee the frequency is configured.
Message: TISCI_MSG_QUERY_FREQ
Request: tisci_msg_query_freq_req
Response: tisci_msg_query_freq_resp
moduleId | Module for which the state should be set. Refer Sciclient_PmDeviceIds. |
clockId | Clock Id for the module. Refer Sciclient_PmModuleClockIds. |
reqFreqHz | The target clock frequency. |
respFreqHz | The frequency that the hardware would set for the given parameters. |
timeout | Gives a sense of how long to wait for the operation. Refer Sciclient_ServiceOperationTimeout. |
int32_t Sciclient_pmQueryModuleClkFreqRange | ( | uint32_t | moduleId, |
uint32_t | clockId, | ||
uint64_t | reqFreqHz, | ||
uint64_t | minFreqHz, | ||
uint64_t | maxFreqHz, | ||
uint64_t * | respFreqHz, | ||
uint32_t | timeout | ||
) |
Message to query the best clock frequency in the given range. This message does no real operation, instead, it requests the system control entity to respond with the best frequency that can match a frequency range provided. NOTE: This is a snapshot view. In a multi processing system, it is very well possible that another processing entity might change the configuration after one entity has queried for best match capability. Only a SET_CLOCK_FREQ will guarantee the frequency is configured.
Message: TISCI_MSG_QUERY_FREQ
Request: tisci_msg_query_freq_req
Response: tisci_msg_query_freq_resp
moduleId | Module for which the state should be set. Refer Sciclient_PmDeviceIds. |
clockId | Clock Id for the module. Refer Sciclient_PmModuleClockIds. |
reqFreqHz | The target clock frequency. |
minFreqHz | The target clock frequency(Min Limit) |
maxFreqHz | The target clock frequency(Max Limit) |
respFreqHz | The frequency that the hardware would set for the given parameters. |
timeout | Gives a sense of how long to wait for the operation. Refer Sciclient_ServiceOperationTimeout. |
int32_t Sciclient_pmGetModuleClkFreq | ( | uint32_t | moduleId, |
uint32_t | clockId, | ||
uint64_t * | freqHz, | ||
uint32_t | timeout | ||
) |
Message to Get Clock Frequency This is most used functionality and is meant for usage when the driver controlling the hardware block requires to know the input clock frequency for configuring internal dividers / multipliers as required.
Message: TISCI_MSG_GET_FREQ
Request: tisci_msg_get_freq_req
Response: tisci_msg_get_freq_resp
moduleId | Module for which the state should be set. Refer Sciclient_PmDeviceIds. |
clockId | Clock Id for the module. Refer Sciclient_PmModuleClockIds. |
freqHz | Frequency of the clock returned in Hertz. |
timeout | Gives a sense of how long to wait for the operation. Refer Sciclient_ServiceOperationTimeout. |
int32_t Sciclient_pmEnableWdt | ( | uint32_t | timeout | ) |
Enables the WDT controllers within the DMSC.
Message: TISCI_MSG_ENABLE_WDT
Request: tisci_msg_enable_wdt_req
Response: tisci_msg_enable_wdt_resp
timeout | Gives a sense of how long to wait for the operation. Refer Sciclient_ServiceOperationTimeout. |
int32_t Sciclient_pmDisableWakeup | ( | uint32_t | timeout | ) |
This message is part of the CPU Off sequence. The sequence is:
Message: TISCI_MSG_WAKE_RESET
Request: tisci_msg_wake_reset_req
Response: tisci_msg_wake_reset_resp
timeout | Gives a sense of how long to wait for the operation. Refer Sciclient_ServiceOperationTimeout. |
int32_t Sciclient_pmGetWakeupReason | ( | uint8_t | mode[32], |
uint8_t | reason[32], | ||
uint32_t * | time_ms, | ||
uint32_t | timeout | ||
) |
Request wakeup reason After a wakeup, the host can request the deepest sleep/idle mode reached and the reason for the wakeup. The API also returns the time spent in idle state.
Message: TISCI_MSG_WAKE_REASON
Request: tisci_msg_wake_reason_req
Response: tisci_msg_wake_reason_resp
mode | Deepest sleep/idle mode 0x000C reached (ASCII) |
reason | Wakeup reason (ASCII) |
time_ms | Time spent in idle state (ms) |
timeout | Gives a sense of how long to wait for the operation. Refer Sciclient_ServiceOperationTimeout. |
int32_t Sciclient_pmDevicePowerOff | ( | uint32_t | timeout | ) |
Some processors have a special sequence for powering off the core that provides notification to the PMMC when that sequence has completed. For processors without such a sequence, the goodbye message exists. The exact sequence involved in the goodbye message depends on the SoC.
Message: TISCI_MSG_GOODBYE
Request: tisci_msg_goodbye_req
Response: tisci_msg_goodbye_resp
timeout | Gives a sense of how long to wait for the operation. Refer Sciclient_ServiceOperationTimeout. |
int32_t Sciclient_pmDeviceReset | ( | uint32_t | timeout | ) |
Objective: Trigger a SoC level reset Usage: Used to trigger a system level reset. NOTE: Depending on permissions configured for the SoC, not all processing entities may be permitted to request a SoC reset. When permitted, the request once processed will not return back to caller.
Message: TISCI_MSG_SYS_RESET
Request: tisci_msg_sys_reset_req
Response: tisci_msg_sys_reset_resp
timeout | Gives a sense of how long to wait for the operation. Refer Sciclient_ServiceOperationTimeout. |
int32_t Sciclient_pmDomainReset | ( | domgrp_t | domGrp, |
uint32_t | timeout | ||
) |
Objective: Trigger a SoC level reset to parts of the SoC.
Message: TISCI_MSG_SYS_RESET
Request: tisci_msg_sys_reset_req
Response: tisci_msg_sys_reset_resp
domGrp | Domain group to reset |
timeout | Gives a sense of how long to wait for the operation. Refer Sciclient_ServiceOperationTimeout. |
int32_t Sciclient_pmIsModuleValid | ( | uint32_t | modId | ) |
This API would check if the given module Id is valid for the device.
modId | Module Index to be checked. |