![]() |
PDK API Guide for J721E
|
SemaphoreP interface
Files | |
file | SemaphoreP.h |
Semaphore module for the RTOS Porting Interface. | |
Data Structures | |
struct | SemaphoreP_Params |
Basic SemaphoreP Parameters. More... | |
Functions | |
SemaphoreP_Handle | SemaphoreP_create (uint32_t count, const SemaphoreP_Params *semParams) |
Function to create a semaphore. More... | |
SemaphoreP_Status | SemaphoreP_delete (SemaphoreP_Handle semPhandle) |
Function to delete a semaphore. More... | |
void | SemaphoreP_Params_init (SemaphoreP_Params *semParams) |
Initialize params structure to default values. More... | |
SemaphoreP_Status | SemaphoreP_pend (SemaphoreP_Handle semPhandle, uint32_t timeout) |
Function to pend (wait) on a semaphore. More... | |
SemaphoreP_Status | SemaphoreP_post (SemaphoreP_Handle semPhandle) |
Function to post (signal) a semaphore. More... | |
SemaphoreP_Status | SemaphoreP_postFromClock (SemaphoreP_Handle semPhandle) |
Function to post (signal) a semaphore from an ClockP function. More... | |
SemaphoreP_Status | SemaphoreP_postFromISR (SemaphoreP_Handle semPhandle) |
Function to post (signal) a semaphore from an ISR. More... | |
int32_t | SemaphoreP_getCount (SemaphoreP_Handle semPhandle) |
Function to return the count of a semaphore. More... | |
SemaphoreP_Status | SemaphoreP_reset (SemaphoreP_Handle semPhandle) |
Function to clear a semaphore for reuse. More... | |
Typedefs | |
typedef void * | SemaphoreP_Handle |
Opaque client reference to an instance of a SemaphoreP. More... | |
Macros | |
#define | SemaphoreP_WAIT_FOREVER (~((uint32_t)0U)) |
Wait forever define. More... | |
#define | SemaphoreP_NO_WAIT ((uint32_t)0U) |
No wait define. More... | |
Semaphore status code | |
typedef int32_t | SemaphoreP_Status |
Status codes for SemaphoreP APIs. More... | |
#define | SemaphoreP_OK (0) |
#define | SemaphoreP_FAILURE (-(int32_t)1) |
#define | SemaphoreP_TIMEOUT (-(int32_t)2) |
#define | SemaphoreP_UNSUPPORTED (-(int32_t)3) |
Mode of Semaphore | |
typedef uint32_t | SemaphoreP_Mode |
Mode of the semaphore. More... | |
#define | SemaphoreP_Mode_COUNTING (0x0U) |
#define | SemaphoreP_Mode_BINARY (0x1U) |
#define SemaphoreP_OK (0) |
#define SemaphoreP_FAILURE (-(int32_t)1) |
API completed successfully
#define SemaphoreP_TIMEOUT (-(int32_t)2) |
API failed
#define SemaphoreP_UNSUPPORTED (-(int32_t)3) |
API failed because of a timeout
#define SemaphoreP_WAIT_FOREVER (~((uint32_t)0U)) |
Wait forever define.
API failed because of not supported
#define SemaphoreP_NO_WAIT ((uint32_t)0U) |
No wait define.
#define SemaphoreP_Mode_COUNTING (0x0U) |
#define SemaphoreP_Mode_BINARY (0x1U) |
typedef int32_t SemaphoreP_Status |
Status codes for SemaphoreP APIs.
typedef void* SemaphoreP_Handle |
Opaque client reference to an instance of a SemaphoreP.
A SemaphoreP_Handle returned from the SemaphoreP_create represents that instance and is used in the other instance based functions (e.g. SemaphoreP_post or SemaphoreP_pend, etc.).
typedef uint32_t SemaphoreP_Mode |
Mode of the semaphore.
SemaphoreP_Handle SemaphoreP_create | ( | uint32_t | count, |
const SemaphoreP_Params * | semParams | ||
) |
Function to create a semaphore.
count | Initial count of the semaphore. For binary semaphores, only values of 0 or 1 are valid. |
semParams | Pointer to the instance configuration parameters. NULL denotes to use the default parameters (SemaphoreP default parameters as noted in SemaphoreP_Params_init. |
SemaphoreP_Status SemaphoreP_delete | ( | SemaphoreP_Handle | semPhandle | ) |
Function to delete a semaphore.
semPhandle | A SemaphoreP_Handle returned from SemaphoreP_create |
void SemaphoreP_Params_init | ( | SemaphoreP_Params * | semParams | ) |
Initialize params structure to default values.
The default parameters are:
semParams | Pointer to the instance configuration parameters. |
SemaphoreP_Status SemaphoreP_pend | ( | SemaphoreP_Handle | semPhandle, |
uint32_t | timeout | ||
) |
Function to pend (wait) on a semaphore.
semPhandle | A SemaphoreP_Handle returned from SemaphoreP_create |
timeout | Timeout (in milliseconds) to wait for the semaphore to be posted (signalled). |
SemaphoreP_Status SemaphoreP_post | ( | SemaphoreP_Handle | semPhandle | ) |
Function to post (signal) a semaphore.
semPhandle | A SemaphoreP_Handle returned from SemaphoreP_create |
SemaphoreP_Status SemaphoreP_postFromClock | ( | SemaphoreP_Handle | semPhandle | ) |
Function to post (signal) a semaphore from an ClockP function.
semPhandle | A SemaphoreP_Handle returned from SemaphoreP_create |
SemaphoreP_Status SemaphoreP_postFromISR | ( | SemaphoreP_Handle | semPhandle | ) |
Function to post (signal) a semaphore from an ISR.
semPhandle | A SemaphoreP_Handle returned from SemaphoreP_create |
int32_t SemaphoreP_getCount | ( | SemaphoreP_Handle | semPhandle | ) |
Function to return the count of a semaphore.
semPhandle | A SemaphoreP_Handle returned from SemaphoreP_create |
SemaphoreP_Status SemaphoreP_reset | ( | SemaphoreP_Handle | semPhandle | ) |
Function to clear a semaphore for reuse.
semPhandle | A SemaphoreP_Handle returned from SemaphoreP_create |