![]() |
![]() |
XDAIS
dais-x04
|
Defines the run time output arguments for all IVIDENC1 instance objects. More...
#include <ividenc1.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | extendedError |
Extended error information. | |
XDAS_Int32 | bytesGenerated |
XDAS_Int32 | encodedFrameType |
Video frame types. | |
XDAS_Int32 | inputFrameSkip |
Video frame skipping modes. | |
XDAS_Int32 | outputID |
XDM1_SingleBufDesc | encodedBuf |
IVIDEO1_BufDesc | reconBufs |
Defines the run time output arguments for all IVIDENC1 instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.XDAS_Int32 IVIDENC1_OutArgs::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IVIDENC1_OutArgs::extendedError |
Extended error information.
XDAS_Int32 IVIDENC1_OutArgs::bytesGenerated |
Number of bytes generated during the IVIDENC1_Fxns::process() call.
XDAS_Int32 IVIDENC1_OutArgs::encodedFrameType |
Video frame types.
IVIDEO_xy_FRAME
values, this frame type is interlaced where both top and bottom fields are provided in a single frame. The first field is an "x" frame, the second field is "y" field.XDAS_Int32 IVIDENC1_OutArgs::inputFrameSkip |
Video frame skipping modes.
XDAS_Int32 IVIDENC1_OutArgs::outputID |
Output ID corresponding with the encoded buffer. This shall also be used to free up the corresponding image buffer for further use by client application code.
XDM1_SingleBufDesc IVIDENC1_OutArgs::encodedBuf |
The encoder fills the buffer with the encoded bitstream. In case of sequences having I & P frames only, these values are identical to outBufs
passed in IVIDENC1_Fxns::process().
encodedBuf.bufSize
field returned corresponds to the actual valid size of the memory buffer. See the bytesGenerated
field for how much data is in this buffer.outputID
and encodedBuf
together provide info relating to the corresponding encoded image buffer. IVIDEO1_BufDesc IVIDENC1_OutArgs::reconBufs |
Reconstruction frames.
outBufs->bufs
[1], outBufs->bufs
[2], and outBufs->bufs
[3].reconBufs.bufDesc
[0].buf is equivalent to outBufs->bufs
[1], reconBufs.bufDesc
[1].buf is equivalent to outBufs->bufs
[2], and reconBufs.bufDesc
[2].buf is equivalent to outBufs->bufs
[3].