![]() |
![]() |
XDAIS
dais-x04
|
Defines the creation time parameters for all IVIDDEC instance objects. More...
#include <ividdec.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | maxHeight |
XDAS_Int32 | maxWidth |
XDAS_Int32 | maxFrameRate |
XDAS_Int32 | maxBitRate |
XDAS_Int32 | dataEndianness |
XDAS_Int32 | forceChromaFormat |
Defines the creation time parameters for all IVIDDEC instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. XDAS_Int32 IVIDDEC_Params::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IVIDDEC_Params::maxHeight |
Maximum video height in pixels.
XDAS_Int32 IVIDDEC_Params::maxWidth |
Maximum video width in pixels.
XDAS_Int32 IVIDDEC_Params::maxFrameRate |
Maximum frame rate in fps * 1000.
XDAS_Int32 IVIDDEC_Params::maxBitRate |
Maximum bit rate, bits per second. For example, if bit rate is 10 Mbps, set this field to 10000000
XDAS_Int32 IVIDDEC_Params::dataEndianness |
Endianness of input data.
XDAS_Int32 IVIDDEC_Params::forceChromaFormat |
Force decode in given Chroma format.