![]() |
![]() |
XDAIS
dais-x04
|
Defines the input arguments for all IVIDANALYTICS instance process function. More...
#include <ividanalytics.h>
Data Fields | |
XDAS_Int32 | size |
XDM_Date | date |
Defines the input arguments for all IVIDANALYTICS instance process function.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.XDAS_Int32 IVIDANALYTICS_InArgs::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDM_Date IVIDANALYTICS_InArgs::date |
Set the current time.