![]() |
![]() |
XDAIS
dais-x04
|
Defines the input arguments for all ISPHDEC instance process function. More...
#include <isphdec.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | frameType |
XDAS_Int32 | inBufferSize |
XDAS_Int32 | bfiFlag |
Defines the input arguments for all ISPHDEC instance process function.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.XDAS_Int32 ISPHDEC_InArgs::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 ISPHDEC_InArgs::frameType |
Input frame type.
XDAS_Int32 ISPHDEC_InArgs::inBufferSize |
Size of valid input data in bytes to be processed.
XDAS_Int32 ISPHDEC_InArgs::bfiFlag |
Bad frame indicator. BFI = 1 indicates bad frame.