![]() |
![]() |
XDAIS
dais-x04
|
Defines the creation time parameters for all IIMGENC1 instance objects. More...
#include <iimgenc1.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | maxHeight |
XDAS_Int32 | maxWidth |
XDAS_Int32 | maxScans |
XDAS_Int32 | dataEndianness |
XDAS_Int32 | forceChromaFormat |
Defines the creation time parameters for all IIMGENC1 instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. XDAS_Int32 IIMGENC1_Params::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IIMGENC1_Params::maxHeight |
Maximum image height.
XDAS_Int32 IIMGENC1_Params::maxWidth |
Maximum image width.
XDAS_Int32 IIMGENC1_Params::maxScans |
Maximum number of scans.
XDAS_Int32 IIMGENC1_Params::dataEndianness |
Endianness of output data.
XDAS_Int32 IIMGENC1_Params::forceChromaFormat |
Force encoding in given Chroma format.