![]() |
![]() |
XDAIS
dais-x04
|
This structure defines the codec parameters that can be modified after creation via control() calls. More...
#include <iimgdec.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | numAU |
XDAS_Int32 | decodeHeader |
Decode entire access unit or only header. | |
XDAS_Int32 | displayWidth |
This structure defines the codec parameters that can be modified after creation via control() calls.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.XDAS_Int32 IIMGDEC_DynamicParams::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IIMGDEC_DynamicParams::numAU |
Number of Access unit to decode. Set to XDM_DEFAULT to decode the entire frame.
XDAS_Int32 IIMGDEC_DynamicParams::decodeHeader |
Decode entire access unit or only header.
XDAS_Int32 IIMGDEC_DynamicParams::displayWidth |
Pitch. If set to zero, imageWidth is used; else, this field (assuming it's larger than imageWidth) is used.