Functions
VXLIB_normL2_i16s_i16s_o16u

Functions

VXLIB_STATUS VXLIB_normL2_i16s_i16s_o16u (const int16_t src_x[restrict], const VXLIB_bufParams2D_t *src_x_addr, const int16_t src_y[restrict], const VXLIB_bufParams2D_t *src_y_addr, uint16_t dst[restrict], const VXLIB_bufParams2D_t *dst_addr)
 
VXLIB_STATUS VXLIB_normL2_i16s_i16s_o16u_checkParams (const int16_t src_x[restrict], const VXLIB_bufParams2D_t *src_x_addr, const int16_t src_y[restrict], const VXLIB_bufParams2D_t *src_y_addr, uint16_t dst[restrict], const VXLIB_bufParams2D_t *dst_addr)
 

Detailed Description

Function Documentation

◆ VXLIB_normL2_i16s_i16s_o16u()

VXLIB_STATUS VXLIB_normL2_i16s_i16s_o16u ( const int16_t  src_x[restrict],
const VXLIB_bufParams2D_t *  src_x_addr,
const int16_t  src_y[restrict],
const VXLIB_bufParams2D_t *  src_y_addr,
uint16_t  dst[restrict],
const VXLIB_bufParams2D_t *  dst_addr 
)
Description:
Computes the L2 norm given 2 16-bit signed inputs, resulting in an unsigned 16-bit norm result.
Method:
The L2 norm is computed using the following equation:
 dst(x,y) = round( sqrt( (src_x(x,y)^2) + (src_y(x,y)^2) ) )
Parameters
[in]src_x[]Pointer to array containing first input image (SQ15.0)
[in]src_x_addr[]Pointer to structure containing dimensional information of src0
[in]src_y[]Pointer to array containing second input image (SQ15.0)
[in]src_y_addr[]Pointer to structure containing dimensional information of src1
[out]dst[]Pointer to array containing output image (UQ15.0)
[in]dst_addr[]Pointer to structure containing dimensional information of dst
Assumptions:
  • I/O buffer pointers are assumed to be not aliased.
Performance Considerations:
  • For best performance, the following parameter settings are recommended:
    • Set widths equal to strides
    • Align all pointers to 8 byte boundaries
    • Set all stride values to a multiple of 8
    • Set all width values to a multiple of 8

◆ VXLIB_normL2_i16s_i16s_o16u_checkParams()

VXLIB_STATUS VXLIB_normL2_i16s_i16s_o16u_checkParams ( const int16_t  src_x[restrict],
const VXLIB_bufParams2D_t *  src_x_addr,
const int16_t  src_y[restrict],
const VXLIB_bufParams2D_t *  src_y_addr,
uint16_t  dst[restrict],
const VXLIB_bufParams2D_t *  dst_addr 
)
Description:
Checks the parameters for programming errors for the VXLIB_normL2_i16s_i16s_o16u function.
Method:
The following checks are made:
  • There shall be no NULL pointers
  • All images shall have the same x and y dimensions
  • The strides of each image shall be equal to or greater than the x dimension
Parameters
[in]src_x[]Pointer to array containing first input image (SQ15.0)
[in]src_x_addr[]Pointer to structure containing dimensional information of src0
[in]src_y[]Pointer to array containing second input image (SQ15.0)
[in]src_y_addr[]Pointer to structure containing dimensional information of src1
[out]dst[]Pointer to array containing output image (UQ15.0)
[in]dst_addr[]Pointer to structure containing dimensional information of dst

Copyright 2022, Texas Instruments Incorporated