Functions
VXLIB_accumulateWeightedImage_i8u_io8u

Functions

VXLIB_STATUS VXLIB_accumulateWeightedImage_i8u_io8u (const uint8_t src[restrict], const VXLIB_bufParams2D_t *src_addr, uint8_t dst[restrict], const VXLIB_bufParams2D_t *dst_addr, VXLIB_F32 alpha)
 
VXLIB_STATUS VXLIB_accumulateWeightedImage_i8u_io8u_checkParams (const uint8_t src[], const VXLIB_bufParams2D_t *src_addr, const uint8_t dst[], const VXLIB_bufParams2D_t *dst_addr, VXLIB_F32 alpha)
 

Detailed Description

Function Documentation

◆ VXLIB_accumulateWeightedImage_i8u_io8u()

VXLIB_STATUS VXLIB_accumulateWeightedImage_i8u_io8u ( const uint8_t  src[restrict],
const VXLIB_bufParams2D_t *  src_addr,
uint8_t  dst[restrict],
const VXLIB_bufParams2D_t *  dst_addr,
VXLIB_F32  alpha 
)
Description:
Accumulates a weighted value from an input image to an output image.
Method:
Weighted accumulation is computed by:
 dst(x,y) = (1alpha)*dst(x,y) + alpha*src(x,y)
Parameters
[in]src[]Pointer to array containing first input image (UQ8.0)
[in]src_addr[]Pointer to structure containing dimensional information of src
[in,out]dst[]Pointer to array containing output image (UQ8.0)
[in]dst_addr[]Pointer to structure containing dimensional information of dst
[in]alphaParameter indicating weight for src and dst (0.0 <= alpha <= 1.0)
Assumptions:
  • I/O buffer pointers are assumed to be not aliased.
Performance Considerations:
  • For best performance, the following parameter settings are recommended:
    • Set widths equal to strides
    • Align all pointers to 8 byte boundaries
    • Set all stride values to a multiple of 8
    • Set all width values to a multiple of 8

◆ VXLIB_accumulateWeightedImage_i8u_io8u_checkParams()

VXLIB_STATUS VXLIB_accumulateWeightedImage_i8u_io8u_checkParams ( const uint8_t  src[],
const VXLIB_bufParams2D_t *  src_addr,
const uint8_t  dst[],
const VXLIB_bufParams2D_t *  dst_addr,
VXLIB_F32  alpha 
)
Description:
Checks the parameters for programming errors for the VXLIB_accumulateImage_i8u_io16s function.
Method:
The following checks are made:
  • There shall be no NULL pointers
  • All images shall have the same x and y dimensions
  • The strides of each image shall be equal to or greater than the x dimension
  • The alpha parameter shall be (0.0 <= alpha <= 1.0)
Parameters
[in]src[]Pointer to array containing first input image (UQ8.0)
[in]src_addr[]Pointer to structure containing dimensional information of src
[in,out]dst[]Pointer to array containing output image (UQ8.0)
[in]dst_addr[]Pointer to structure containing dimensional information of dst
[in]alphaParameter indicating weight for src and dst (0.0 <= alpha <= 1.0)

Copyright 2022, Texas Instruments Incorporated