Vision Apps User Guide

Introduction

This section documents the kernels which are targted to be examples of writing different kernels.

Files

file  tivx_sample_kernels.h
 The list of supported kernels in this kernel extension.
 

Data Structures

struct  tivx_pcie_tx_params_t
 PCIe TX Node parameters. More...
 
struct  tivx_pcie_rx_params_t
 PCIe RX Node parameters. More...
 
struct  tivx_opengl_mosaic_params_t
 OpenGL Mosaic Node parameters. More...
 

Functions

void tivxSampleLoadKernels (vx_context context)
 Used for the Application to load the sample kernels into the context. More...
 
void tivxSampleUnLoadKernels (vx_context context)
 Used for the Application to unload the sample kernels from the context. More...
 
void tivxSamplePrintPerformance (vx_perf_t performance, uint32_t numPixels, const char *testName)
 Used to print the performance of the kernels. More...
 
VX_API_ENTRY vx_node VX_API_CALL tivxOpenglMosaicNode (vx_graph graph, vx_user_data_object configuration, vx_object_array input, vx_image output)
 [Graph] Creates a OPENGL_MOSAIC Node. More...
 
VX_API_ENTRY vx_node VX_API_CALL tivxPcieTxNode (vx_graph graph, vx_user_data_object configuration, vx_image input)
 [Graph] Creates a PCIE_TX Node. More...
 
VX_API_ENTRY vx_node VX_API_CALL tivxPcieRxNode (vx_graph graph, vx_user_data_object configuration, vx_object_array output)
 [Graph] Creates a PCIE_RX Node. More...
 

Macros

#define TIVX_MODULE_NAME_SAMPLE   "sample"
 Name for OpenVX Extension kernel module: sample. More...
 
#define TIVX_KERNEL_OPENGL_MOSAIC_NAME   "com.ti.sample.opengl_mosaic"
 The list of kernels supported in sample module. More...
 
#define TIVX_KERNEL_PCIE_TX_NAME   "com.ti.sample.pcie_tx"
 pcie_tx kernel name More...
 
#define TIVX_KERNEL_PCIE_RX_NAME   "com.ti.sample.pcie_rx"
 pcie_rx kernel name More...
 
#define TIVX_KERNEL_PCIE_TX_MAX_CHANNELS   (1U)
 Maximum channels supported by an instance of PCIe TX kernel. More...
 
#define TIVX_PCIE_RX_MIN_PIPEUP_BUFS   (3U)
 Minimum pipe-up buffers needed for an instance of PCIe RX kernel. More...
 
#define TIVX_KERNEL_PCIE_RX_MAX_CHANNELS   (1U)
 Maximum channels supported by an instance of PCIe RX kernel. More...
 
#define TIVX_KERNEL_OPENGL_MOSAIC_TYPE_1x1   (0)
 The configuration data structure used by the TIVX_KERNEL_OPENGL_MOSAIC kernel. More...
 
#define TIVX_KERNEL_OPENGL_MOSAIC_TYPE_2x2   (1)
 

Macro Definition Documentation

◆ TIVX_MODULE_NAME_SAMPLE

#define TIVX_MODULE_NAME_SAMPLE   "sample"

Name for OpenVX Extension kernel module: sample.

◆ TIVX_KERNEL_OPENGL_MOSAIC_NAME

#define TIVX_KERNEL_OPENGL_MOSAIC_NAME   "com.ti.sample.opengl_mosaic"

The list of kernels supported in sample module.

Each kernel listed here can be used with the vxGetKernelByName call. When programming the parameters, use

  • VX_INPUT for [in]
  • VX_OUTPUT for [out]
  • VX_BIDIRECTIONAL for [in,out]

When programming the parameters, use

  • VX_TYPE_IMAGE for a vx_image in the size field of vxGetParameterByIndex or vxSetParameterByIndex
  • VX_TYPE_ARRAY for a vx_array in the size field of vxGetParameterByIndex or vxSetParameterByIndex
  • or other appropriate types in vx_type_e.

opengl_mosaic kernel name

◆ TIVX_KERNEL_PCIE_TX_NAME

#define TIVX_KERNEL_PCIE_TX_NAME   "com.ti.sample.pcie_tx"

pcie_tx kernel name

◆ TIVX_KERNEL_PCIE_RX_NAME

#define TIVX_KERNEL_PCIE_RX_NAME   "com.ti.sample.pcie_rx"

pcie_rx kernel name

◆ TIVX_KERNEL_PCIE_TX_MAX_CHANNELS

#define TIVX_KERNEL_PCIE_TX_MAX_CHANNELS   (1U)

Maximum channels supported by an instance of PCIe TX kernel.

◆ TIVX_PCIE_RX_MIN_PIPEUP_BUFS

#define TIVX_PCIE_RX_MIN_PIPEUP_BUFS   (3U)

Minimum pipe-up buffers needed for an instance of PCIe RX kernel.

◆ TIVX_KERNEL_PCIE_RX_MAX_CHANNELS

#define TIVX_KERNEL_PCIE_RX_MAX_CHANNELS   (1U)

Maximum channels supported by an instance of PCIe RX kernel.

◆ TIVX_KERNEL_OPENGL_MOSAIC_TYPE_1x1

#define TIVX_KERNEL_OPENGL_MOSAIC_TYPE_1x1   (0)

The configuration data structure used by the TIVX_KERNEL_OPENGL_MOSAIC kernel.

< Mosaic/Render Type - 1x1 (single window) mosaic Mosaic/Render Type - 2x2 (4 window) mosaic

◆ TIVX_KERNEL_OPENGL_MOSAIC_TYPE_2x2

#define TIVX_KERNEL_OPENGL_MOSAIC_TYPE_2x2   (1)

Function Documentation

◆ tivxSampleLoadKernels()

void tivxSampleLoadKernels ( vx_context  context)

Used for the Application to load the sample kernels into the context.

◆ tivxSampleUnLoadKernels()

void tivxSampleUnLoadKernels ( vx_context  context)

Used for the Application to unload the sample kernels from the context.

◆ tivxSamplePrintPerformance()

void tivxSamplePrintPerformance ( vx_perf_t  performance,
uint32_t  numPixels,
const char *  testName 
)

Used to print the performance of the kernels.

◆ tivxOpenglMosaicNode()

VX_API_ENTRY vx_node VX_API_CALL tivxOpenglMosaicNode ( vx_graph  graph,
vx_user_data_object  configuration,
vx_object_array  input,
vx_image  output 
)

[Graph] Creates a OPENGL_MOSAIC Node.

Parameters
[in]graphThe reference to the graph.
[in]configuration
[in]input
[out]output
See also
TIVX_KERNEL_OPENGL_MOSAIC_NAME
Returns
vx_node.
Return values
vx_nodeA node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus

◆ tivxPcieTxNode()

VX_API_ENTRY vx_node VX_API_CALL tivxPcieTxNode ( vx_graph  graph,
vx_user_data_object  configuration,
vx_image  input 
)

[Graph] Creates a PCIE_TX Node.

Parameters
[in]graphThe reference to the graph.
[in]configuration
[in]input
See also
TIVX_KERNEL_PCIE_TX_NAME
Returns
vx_node.
Return values
vx_nodeA node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus

◆ tivxPcieRxNode()

VX_API_ENTRY vx_node VX_API_CALL tivxPcieRxNode ( vx_graph  graph,
vx_user_data_object  configuration,
vx_object_array  output 
)

[Graph] Creates a PCIE_RX Node.

Parameters
[in]graphThe reference to the graph.
[in]configuration
[out]output
See also
TIVX_KERNEL_PCIE_RX_NAME
Returns
vx_node.
Return values
vx_nodeA node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus