![]() |
TI Deep Learning Product User Guide
|
This structure define the parameters of Element wise layer in TIDL.
Data Fields | |
int32_t | bias |
int32_t | numChannels |
int32_t | eltWiseType |
int32_t | numInData |
int32_t | biasQ |
int32_t | inDataQ [TIDL_NUM_IN_BUFS] |
int32_t | outDataQ |
int32_t sTIDL_EltWiseParams_t::bias |
Offset for bias parameters
int32_t sTIDL_EltWiseParams_t::numChannels |
Number of channels channels to be processed
int32_t sTIDL_EltWiseParams_t::eltWiseType |
Type of the element wise operation
int32_t sTIDL_EltWiseParams_t::numInData |
Number of input data buffers on which EltWise operation will be done
int32_t sTIDL_EltWiseParams_t::biasQ |
Q value kernel Bias
int32_t sTIDL_EltWiseParams_t::inDataQ[TIDL_NUM_IN_BUFS] |
Q value of the in data buffers
int32_t sTIDL_EltWiseParams_t::outDataQ |
Q value expected for out data