![]() |
TI Deep Learning Product User Guide
|
This structure define the parameters of data or kernel buffer memory in TIDL.
ptr | Address pointing to the actual buffer |
bufSize | Size of the buffer in bytes |
Data Fields | |
void * | ptr |
int32_t | bufSize |
int32_t | reserved [2] |
void* sBuffer_t::ptr |
int32_t sBuffer_t::bufSize |
int32_t sBuffer_t::reserved[2] |