![]() |
TI Autonomous Driving Algorithms (TIADALG) Library User Guide
|
This file defines the interface for pose estimation using pnp technique. More...
#include <tiadalg_interface.h>
Go to the source code of this file.
#define | EXTERNC |
EXTERNC int32_t | tiadalg_solve_pnp_cn (tiadalg_p3p_params *params, float R[3][3], float tvec[3], const float twoDPoints[][2], const float threeDPoints[][3], const int numberOfpoints) |
This API does camera pose estimation using p3p operations. More... | |
EXTERNC int32_t | tiadalg_solve_pnp_c66 (tiadalg_p3p_params *params, float R[3][3], float tvec[3], const float twoDPoints[][2], const float threeDPoints[][3], const int numberOfpoints) |
It does camera pose estimation using solve pnp technique. More... | |
This file defines the interface for pose estimation using pnp technique.
#define EXTERNC |
EXTERNC int32_t tiadalg_solve_pnp_cn | ( | tiadalg_p3p_params * | params, |
float | R[3][3], | ||
float | tvec[3], | ||
const float | twoDPoints[][2], | ||
const float | threeDPoints[][3], | ||
const int | numberOfpoints | ||
) |
This API does camera pose estimation using p3p operations.
tiadalg_solve_pnp_cn
params | [in] : Control parameters for p3p operations. refer tiadalg_p3p_params |
R | [out] : Output 3x3 rotation matrix |
tvec | [out] : Output 3x1 translation matrix [tx,ty,tz] |
twoDPoints | [in] : List of 2d points. x, and y co-ordinates are interleaved |
threeDPoints | [in] : List of coresponding 3d points. X,Y,Z are interleaved |
numberOfpoints | [in] : Total number of matching 2d and 3d points |
EXTERNC int32_t tiadalg_solve_pnp_c66 | ( | tiadalg_p3p_params * | params, |
float | R[3][3], | ||
float | tvec[3], | ||
const float | twoDPoints[][2], | ||
const float | threeDPoints[][3], | ||
const int | numberOfpoints | ||
) |
It does camera pose estimation using solve pnp technique.
tiadalg_solve_pnp_c66
params | [in] : Control parameters for p3p operations. refer tiadalg_p3p_params |
R | [out] : Output 3x3 rotation matrix |
tvec | [out] : Output 3x1 translation matrix [tx,ty,tz] |
twoDPoints | [in] : List of 2d points. x, and y co-ordinates are interleaved |
threeDPoints | [in] : List of coresponding 3d points. X,Y,Z are interleaved |
numberOfpoints | [in] : Total number of matching 2d and 3d points |
|
© Copyright 2018 Texas Instruments Incorporated. All rights reserved. |
Document generated by doxygen 1.8.6 |