![]() |
SDL API Guide for J721E
|
Header file contains enumerations, structure definitions and function.
Go to the source code of this file.
Data Structures | |
struct | SDL_ECC_InitConfig_t |
This structure defines the elements of ECC Init configuration More... | |
struct | SDL_ECC_InjectErrorConfig_t |
This structure defines the inject error configuration More... | |
struct | SDL_ECC_ErrorInfo_t |
This structure defines the error status information More... | |
Typedefs | |
typedef uint32_t | SDL_ECC_MemType |
This enumerator indicate ECC memory type. More... | |
typedef uint32_t | SDL_ECC_MemSubType |
This enumerator indicate ECC memory Sub Type. More... | |
typedef void(* | SDL_ECC_ErrorCallback_t) (uint32_t errorSrc, uint32_t address) |
typedef void(* | SDL_ECC_VIMDEDVector_t) (void) |
Enumerations | |
enum | SDL_ECC_AggregatorType { SDL_ECC_AGGR_TYPE_INJECT_ONLY = 1, SDL_ECC_AGGR_TYPE_FULL_FUNCTION = 2 } |
This enumerator defines the different ECC aggregator types More... | |
enum | SDL_ECC_InjectErrorType { SDL_INJECT_ECC_NO_ERROR = 0, SDL_INJECT_ECC_ERROR_FORCING_1BIT_ONCE = 1, SDL_INJECT_ECC_ERROR_FORCING_2BIT_ONCE = 2, SDL_INJECT_ECC_ERROR_FORCING_1BIT_N_ROW_ONCE = 3, SDL_INJECT_ECC_ERROR_FORCING_2BIT_N_ROW_ONCE = 4, SDL_INJECT_ECC_ERROR_FORCING_1BIT_REPEAT = 5, SDL_INJECT_ECC_ERROR_FORCING_2BIT_REPEAT = 6, SDL_INJECT_ECC_ERROR_FORCING_1BIT_N_ROW_REPEAT = 7, SDL_INJECT_ECC_ERROR_FORCING_2BIT_N_ROW_REPEAT = 8 } |
ECC Inject error types. More... | |
enum | SDL_ECC_RamIdType { SDL_ECC_RAM_ID_TYPE_WRAPPER = 0, SDL_ECC_RAM_ID_TYPE_INTERCONNECT = 1 } |
This enumerator defines the different ECC RAM ID types More... | |
Functions | |
int32_t | SDL_ECC_initEsm (const SDL_ESM_Inst esmInstType) |
Initializes an module for usage with ECC module. More... | |
int32_t | SDL_ECC_init (SDL_ECC_MemType eccMemType, const SDL_ECC_InitConfig_t *pECCInitConfig) |
Initializes ECC module for ECC detection. More... | |
int32_t | SDL_ECC_initMemory (SDL_ECC_MemType eccMemType, SDL_ECC_MemSubType memSubType) |
Initializes Memory to be ready for ECC error detection. Assumes ECC is already enabled. More... | |
int32_t | SDL_ECC_selfTest (SDL_ECC_MemType eccMemType, SDL_ECC_MemSubType memSubType, SDL_ECC_InjectErrorType errorType, const SDL_ECC_InjectErrorConfig_t *pECCErrorConfig, uint32_t selfTestTimeOut) |
Runs self test by injecting and error and monitor response Assumes ECC is already enabled. More... | |
int32_t | SDL_ECC_injectError (SDL_ECC_MemType eccMemType, SDL_ECC_MemSubType memSubType, SDL_ECC_InjectErrorType errorType, const SDL_ECC_InjectErrorConfig_t *pECCErrorConfig) |
Injects ECC error at specified location Assumes ECC is already enabled. More... | |
int32_t | SDL_ECC_getStaticRegisters (SDL_ECC_MemType eccMemType, SDL_ECC_staticRegs *pStaticRegs) |
Gets the static registers for the specified ECC instance. More... | |
int32_t | SDL_ECC_getErrorInfo (SDL_ECC_MemType eccMemType, SDL_Ecc_AggrIntrSrc intrSrc, SDL_ECC_ErrorInfo_t *pErrorInfo) |
Retrieves the ECC error information for the specified memtype and interrupt source. More... | |
int32_t | SDL_ECC_ackIntr (SDL_ECC_MemType eccMemType, SDL_Ecc_AggrIntrSrc intrSrc) |
Acknowledge the ECC interrupt. More... | |
int32_t | SDL_ECC_getESMErrorInfo (SDL_ESM_Inst instance, uint32_t intSrc, SDL_ECC_MemType *eccMemType, SDL_Ecc_AggrIntrSrc *intrSrcType) |
Retrieves the ECC error information for the specified ESM error. If it isn't an ECC error or the ECC error is not supported an error is returned. More... | |
int32_t | SDL_ECC_clearNIntrPending (SDL_ECC_MemType eccMemType, SDL_ECC_MemSubType memSubType, SDL_Ecc_AggrIntrSrc intrSrc, SDL_Ecc_AggrEDCErrorSubType subType, uint32_t numEvents) |
Clears N pending interrupts for the specified memtype, subtype and interrupt source. More... | |
void | SDL_ECC_registerVIMDEDHandler (SDL_ECC_VIMDEDVector_t VIMDEDHandler) |
Register Handler for VIM DED ECC error. More... | |
void | SDL_ECC_applicationCallbackFunction (SDL_ECC_MemType eccMemType, uint32_t errorSrc, uint32_t address, uint32_t ramId, uint64_t bitErrorOffset, uint32_t bitErrorGroup) |
Application provided external callback function for ECC handling Called inside the reference functions when ECC errors occur. NOTE: This is application supplied and not part of the SDL If not supplied by application this will result in an linker error. More... | |