![]() |
SDL API Guide for J721E
|
This file contains the SDL-FL API's for LBIST.
Go to the source code of this file.
Data Structures | |
struct | SDL_LBIST_config_t |
This structure contains the different configuration used for LBIST Note that the LBIST configuration is SOC and instance specific Check SOC documentation for configuration details. More... | |
Functions | |
int32_t | SDL_LBIST_enableIsolation (SDL_lbistRegs *pLBISTRegs) |
Enable LBIST Isolation. More... | |
int32_t | SDL_LBIST_disableIsolation (SDL_lbistRegs *pLBISTRegs) |
Disable LBIST Isolation. More... | |
int32_t | SDL_LBIST_reset (SDL_lbistRegs *pLBISTRegs) |
Reset LBIST. More... | |
int32_t | SDL_LBIST_enableRunBISTMode (SDL_lbistRegs *pLBISTRegs) |
Enable run BIST mode. More... | |
int32_t | SDL_LBIST_clearRunBISTMode (SDL_lbistRegs *pLBISTRegs) |
Clear run BIST mode. More... | |
int32_t | SDL_LBIST_start (SDL_lbistRegs *pLBISTRegs) |
LBIST start. More... | |
int32_t | SDL_LBIST_stop (SDL_lbistRegs *pLBISTRegs) |
LBIST stop. More... | |
int32_t | SDL_LBIST_isRunning (const SDL_lbistRegs *pLBISTRegs, bool *pIsRunning) |
LBIST check running. More... | |
int32_t | SDL_LBIST_isDone (const SDL_lbistRegs *pLBISTRegs, bool *pIsDone) |
LBIST check done. More... | |
int32_t | SDL_LBIST_programConfig (SDL_lbistRegs *pLBISTRegs, const SDL_LBIST_config_t *pConfig) |
LBIST Program config. More... | |
int32_t | SDL_LBIST_getMISR (SDL_lbistRegs *pLBISTRegs, uint32_t *pMISRValue) |
LBIST get MISR. More... | |
int32_t | SDL_LBIST_getExpectedMISR (const uint32_t *pLBISTSig, uint32_t *pExpectedMISRValue) |
LBIST get expected MISR. More... | |