![]() |
PDK API Guide for J721E
|
MAC authentication configuration.
Data Fields | |
bool | authModeEn |
uint32_t | macAuthDisMask |
bool CpswAle_MacAuthCfg::authModeEn |
Enable MAC Authorization mode
uint32_t CpswAle_MacAuthCfg::macAuthDisMask |
Disable Port authorization - When set will allow unknown addresses to arrive on a switch in authorization mode. It is intended for device to device network connection on ports which do not require MACSEC encryption