PDK API Guide for J721E
SwiP

Introduction

SwiP interface

Files

file  SwiP.h
 Software Interrupt module for the RTOS Porting Interface.
 

Data Structures

struct  SwiP_Params
 Basic SwiP Parameters. More...
 

Functions

SwiP_Handle SwiP_create (SwiP_Fxn swiFxn, const SwiP_Params *swiPparams)
 Function to create a software interrupt. More...
 
SwiP_Status SwiP_delete (SwiP_Handle *pHandle)
 Function to delete an interrupt on CortexM devices. More...
 
void SwiP_Params_init (SwiP_Params *swiPparams)
 Initialize params structure to default values. More...
 
SwiP_Status SwiP_post (SwiP_Handle swiPhandle)
 Function to post the Swi interrupt. More...
 

Typedefs

typedef void * SwiP_Handle
 SwiP handle of an instance. More...
 
typedef void(* SwiP_Fxn) (uintptr_t arg0, uintptr_t arg1)
 Prototype for the entry function for a software interrupt. More...
 

Enumerations

enum  SwiP_Status { SwiP_OK = 0, SwiP_FAILURE = (-(int32_t)1) }
 Status codes for SwiP APIs. More...
 

Typedef Documentation

◆ SwiP_Handle

typedef void* SwiP_Handle

SwiP handle of an instance.

A SwiP_Handle returned from the SwiP_create represents that instance.

◆ SwiP_Fxn

typedef void(* SwiP_Fxn) (uintptr_t arg0, uintptr_t arg1)

Prototype for the entry function for a software interrupt.

Enumeration Type Documentation

◆ SwiP_Status

Status codes for SwiP APIs.

Enumerator
SwiP_OK 
SwiP_FAILURE 

Function Documentation

◆ SwiP_create()

SwiP_Handle SwiP_create ( SwiP_Fxn  swiFxn,
const SwiP_Params swiPparams 
)

Function to create a software interrupt.

Parameters
swiFxnentry function of the software interrupt
swiPparamsPointer to the instance configuration parameters. NULL denotes to use the default parameters. The SwiP default parameters are noted in SwiP_Params_init.
Returns
SwiP_Handle

◆ SwiP_delete()

SwiP_Status SwiP_delete ( SwiP_Handle pHandle)

Function to delete an interrupt on CortexM devices.

Parameters
pHandlepointer of the handle returned from the SwiP_create call
Returns
SwiP_OK if successfull, SwiP_FAILURE if fail

◆ SwiP_Params_init()

void SwiP_Params_init ( SwiP_Params swiPparams)

Initialize params structure to default values.

Parameters
swiPparamsPointer to the instance configuration parameters.

◆ SwiP_post()

SwiP_Status SwiP_post ( SwiP_Handle  swiPhandle)

Function to post the Swi interrupt.

Parameters
swiPhandleThe swiP handle
Returns
SwiP_OK if successfull, SwiP_FAILURE if fail