TI Deep Learning Product User Guide
|
Data Fields | |
int32_t | slicePoints [TIDL_NUM_OUT_BUFS+1] |
int32_t | axis |
int32_t | stride |
int32_t sTIDL_SliceLayerParams_t::slicePoints[TIDL_NUM_OUT_BUFS+1] |
Num channel in the each out buffer /tensor
int32_t sTIDL_SliceLayerParams_t::axis |
Axis on which the concat is performed
int32_t sTIDL_SliceLayerParams_t::stride |
Stride in Slice axis - Only Supported value is 1