TI Deep Learning Product User Guide
|
This structure define the parameters of Pad layer in TIDL.
Data Fields | |
int32_t | padT |
int32_t | padB |
int32_t | padL |
int32_t | padR |
int32_t | padConstValue |
int32_t | padType |
int32_t | perChannelPadConstTensorOffset |
int32_t sTIDL_PadLayerParams_t::padT |
Top padding to be added as part of the pad layer
int32_t sTIDL_PadLayerParams_t::padB |
Bottom padding to be added as part of the pad layer
int32_t sTIDL_PadLayerParams_t::padL |
Left padding to be added as part of the pad layer
int32_t sTIDL_PadLayerParams_t::padR |
Right padding to be added as part of the pad layer
int32_t sTIDL_PadLayerParams_t::padConstValue |
The value of the constant to be padded to the layer
int32_t sTIDL_PadLayerParams_t::padType |
Type of padding to be done as defined in eTIDL_PadLayerPadType
int32_t sTIDL_PadLayerParams_t::perChannelPadConstTensorOffset |
Offset where per channel values to be used for padding are stored. A value of zero indicates that this infomation is not valid