TI Deep Learning Product User Guide
|
This structure define the common layer parameters in TIDL.
Data Fields | |
sTIDL_LayerParams_t | layerParams |
sTIDL_ActParams_t | actParams |
int32_t | layerType |
int32_t | numInBufs |
int32_t | numOutBufs |
sTIDL_DataParams_t | inData [TIDL_NUM_IN_BUFS] |
sTIDL_DataParams_t | outData [TIDL_NUM_OUT_BUFS] |
int32_t | coreID |
int32_t | layersGroupId |
int32_t | weightsElementSizeInBits |
int32_t | strideOffsetMethod |
sTIDL_LayerParams_t sTIDL_Layer_t::layerParams |
sTIDL_ActParams_t sTIDL_Layer_t::actParams |
Feature activation type used by TIDL layer
int32_t sTIDL_Layer_t::layerType |
Layer Type as defined by eTIDL_LayerType
int32_t sTIDL_Layer_t::numInBufs |
Number of input data buffers for the layer
int32_t sTIDL_Layer_t::numOutBufs |
Number of output data buffers for the layer
sTIDL_DataParams_t sTIDL_Layer_t::inData[TIDL_NUM_IN_BUFS] |
Input data buffers details
sTIDL_DataParams_t sTIDL_Layer_t::outData[TIDL_NUM_OUT_BUFS] |
output data buffers details
int32_t sTIDL_Layer_t::coreID |
Processing core ID
int32_t sTIDL_Layer_t::layersGroupId |
Group of layers in the net are processed together. This unique number identify the currently processing group
int32_t sTIDL_Layer_t::weightsElementSizeInBits |
Size of compute layer weight parameters in bytes
int32_t sTIDL_Layer_t::strideOffsetMethod |
Offset selection method for stride. eTIDL_StrideOffsetMethod