![]() |
SDL API Guide for J721E
|
This structure contains the static register group for Ecc aggregator used by the SDL_ecc_aggrReadStaticRegs function.
Design: PROC_SDL-1281
Data Fields | |
uint32_t | REV |
uint32_t | ECC_CTRL |
uint32_t | ECC_ERR_CTRL1 |
uint32_t | ECC_ERR_CTRL2 |
uint32_t | ECC_SEC_ENABLE_SET_REG [SDL_ECC_AGGR_NUM_ENABLE_REGISTERS] |
uint32_t | ECC_SEC_ENABLE_CLR_REG [SDL_ECC_AGGR_NUM_ENABLE_REGISTERS] |
uint32_t | ECC_DED_ENABLE_SET_REG [SDL_ECC_AGGR_NUM_ENABLE_REGISTERS] |
uint32_t | ECC_DED_ENABLE_CLR_REG [SDL_ECC_AGGR_NUM_ENABLE_REGISTERS] |
uint32_t SDL_ECC_staticRegs::REV |
Aggregator Revision Register
uint32_t SDL_ECC_staticRegs::ECC_CTRL |
ECC Control register
uint32_t SDL_ECC_staticRegs::ECC_ERR_CTRL1 |
ECC Err Control1 register
uint32_t SDL_ECC_staticRegs::ECC_ERR_CTRL2 |
ECC Err Control2 register
uint32_t SDL_ECC_staticRegs::ECC_SEC_ENABLE_SET_REG[SDL_ECC_AGGR_NUM_ENABLE_REGISTERS] |
ECC_SEC_ENABLE_SET_REG registers
uint32_t SDL_ECC_staticRegs::ECC_SEC_ENABLE_CLR_REG[SDL_ECC_AGGR_NUM_ENABLE_REGISTERS] |
ECC_SEC_ENABLE_SET_REG registers
uint32_t SDL_ECC_staticRegs::ECC_DED_ENABLE_SET_REG[SDL_ECC_AGGR_NUM_ENABLE_REGISTERS] |
ECC_DED_ENABLE_SET_REG registers
uint32_t SDL_ECC_staticRegs::ECC_DED_ENABLE_CLR_REG[SDL_ECC_AGGR_NUM_ENABLE_REGISTERS] |
ECC_DED_ENABLE_SET_REG registers