SDL API Guide for J721E
MCU CCMR5 Enumerated Data Types

Introduction

Enumerations

enum  SDL_McuArmssCcmR5RegId {
  SDL_MCU_ARMSS_CCMR5_CCMSR1_REGID = (0u), SDL_MCU_ARMSS_CCMR5_CCMKEYR1_REGID = (1u), SDL_MCU_ARMSS_CCMR5_CCMSR2_REGID = (2u), SDL_MCU_ARMSS_CCMR5_CCMKEYR2_REGID = (3u),
  SDL_MCU_ARMSS_CCMR5_CCMSR3_REGID = (4u), SDL_MCU_ARMSS_CCMR5_CCMKEYR3_REGID = (5u), SDL_MCU_ARMSS_CCMR5_POLCNTRL_REGID = (6u), SDL_MCU_ARMSS_CCMR5_INVALID_REGID = (7u)
}
 This typedef defines the MCU ARMSS CCM R5 register ID type used under the context of SDL CCMR5 APIs. More...
 
enum  SDL_McuArmssCcmR5ModuleId { SDL_MCU_ARMSS_CCMR5_CPU_MODULE_ID = (0u), SDL_MCU_ARMSS_CCMR5_VIM_MODULE_ID = (1u), SDL_MCU_ARMSS_CCMR5_INACTIVITY_MONITOR_MODULE_ID = (2u), SDL_MCU_ARMSS_CCMR5_INVALID_MODULE_ID = (255u) }
 This enum defines the MCU ARMSS CCM R5 module ID type used under the context of SDL CCMR5 APIs. More...
 
enum  SDL_McuArmssCcmR5OpModeKey { SDL_MCU_ARMSS_CCMR5_MKEY_CMP_MODE_ACTIVE = (0u), SDL_MCU_ARMSS_CCMR5_MKEY_SELF_TEST_MODE = (6u), SDL_MCU_ARMSS_CCMR5_MKEY_ERR_FORCE_MODE = (9u), SDL_MCU_ARMSS_CCMR5_MKEY_SELF_TEST_ERR_FORCE_MODE = (15u) }
 This enum defines the MCU ARMSS CCM R5 Operation Mode Key values used under the context of SDL CCMR5 APIs. More...
 

Enumeration Type Documentation

◆ SDL_McuArmssCcmR5RegId

This typedef defines the MCU ARMSS CCM R5 register ID type used under the context of SDL CCMR5 APIs.

Enumerator
SDL_MCU_ARMSS_CCMR5_CCMSR1_REGID 
SDL_MCU_ARMSS_CCMR5_CCMKEYR1_REGID 

register id for Status Register 1

SDL_MCU_ARMSS_CCMR5_CCMSR2_REGID 

register id for KEY register 1

SDL_MCU_ARMSS_CCMR5_CCMKEYR2_REGID 

register id for Status Register 2

SDL_MCU_ARMSS_CCMR5_CCMSR3_REGID 

register id for KEY register 2

SDL_MCU_ARMSS_CCMR5_CCMKEYR3_REGID 

register id for Status Register 3

SDL_MCU_ARMSS_CCMR5_POLCNTRL_REGID 

register id for KEY register 3

SDL_MCU_ARMSS_CCMR5_INVALID_REGID 

register id for Polatiry Control Reg

◆ SDL_McuArmssCcmR5ModuleId

This enum defines the MCU ARMSS CCM R5 module ID type used under the context of SDL CCMR5 APIs.

Enumerator
SDL_MCU_ARMSS_CCMR5_CPU_MODULE_ID 
SDL_MCU_ARMSS_CCMR5_VIM_MODULE_ID 

module id for Cpu

SDL_MCU_ARMSS_CCMR5_INACTIVITY_MONITOR_MODULE_ID 

module id for VIM

SDL_MCU_ARMSS_CCMR5_INVALID_MODULE_ID 

module id for Inactivity monitor

◆ SDL_McuArmssCcmR5OpModeKey

This enum defines the MCU ARMSS CCM R5 Operation Mode Key values used under the context of SDL CCMR5 APIs.

Enumerator
SDL_MCU_ARMSS_CCMR5_MKEY_CMP_MODE_ACTIVE 
SDL_MCU_ARMSS_CCMR5_MKEY_SELF_TEST_MODE 

compare mode active operation Mode key

SDL_MCU_ARMSS_CCMR5_MKEY_ERR_FORCE_MODE 

Self Test active operation Mode key

SDL_MCU_ARMSS_CCMR5_MKEY_SELF_TEST_ERR_FORCE_MODE 

Error Force mode operation Mode key