===========================================================================
|
int32_t | SDL_RTI_getWindowSize (uint32_t baseAddr, uint32_t *pWinSize) |
| This API will return current configured Window Size. More...
|
|
int32_t | SDL_RTI_setPreload (uint32_t baseAddr, uint32_t dwwdPreloadVal) |
| Set DWWD preload value. From this value down counter starts down counting. More...
|
|
int32_t | SDL_RTI_getPreload (uint32_t baseAddr, uint32_t *pPreloadVal) |
| This API will return current configured Preload value. More...
|
|
◆ SDL_RTI_getWindowSize()
int32_t SDL_RTI_getWindowSize |
( |
uint32_t |
baseAddr, |
|
|
uint32_t * |
pWinSize |
|
) |
| |
This API will return current configured Window Size.
- Parameters
-
baseAddr | Base Address of the RTI instance. |
pWinSize | pointer to Configured Window Size. Refer macro RTI_WindowSize_t |
- Returns
- status Success of the window configuration
- Success: SDL_PASS
- Fail : SDL_EFAIL
◆ SDL_RTI_setPreload()
int32_t SDL_RTI_setPreload |
( |
uint32_t |
baseAddr, |
|
|
uint32_t |
dwwdPreloadVal |
|
) |
| |
Set DWWD preload value. From this value down counter starts down counting.
- Parameters
-
baseAddr | Base Address of the RTI instance. |
dwwdPreloadVal | Down counter preload value. Refer DWWD Down Counter Overview. |
- Returns
- status Success of the window configuration
- Success: SDL_PASS
- Fail : SDL_EFAIL
◆ SDL_RTI_getPreload()
int32_t SDL_RTI_getPreload |
( |
uint32_t |
baseAddr, |
|
|
uint32_t * |
pPreloadVal |
|
) |
| |
This API will return current configured Preload value.
- Parameters
-
baseAddr | Base Address of the RTI instance. |
pPreloadVal | pointer to current preload value |
- Returns
- status Success of the window configuration
- Success: SDL_PASS
- Fail : SDL_EFAIL