54 #ifndef MESSAGES_CORE_H 55 #define MESSAGES_CORE_H uint8_t abi_minor
Definition: tisci_core.h:86
uint16_t tisci_boardcfg_size
Definition: tisci_core.h:173
struct tisci_header hdr
Definition: tisci_core.h:67
uint32_t msmc_start_high
Definition: tisci_core.h:284
uint16_t tisci_boardcfg_security_size
Definition: tisci_core.h:206
devgrp_t tisci_boardcfg_devgrp
Definition: tisci_core.h:174
struct tisci_header hdr
Definition: tisci_core.h:186
uint16_t tisci_boardcfg_pm_size
Definition: tisci_core.h:239
struct tisci_header hdr
Definition: tisci_core.h:127
uint32_t tisci_boardcfgp_high
Definition: tisci_core.h:172
struct tisci_header hdr
Definition: tisci_core.h:282
TISCI_MSG_BOARD_CONFIG_RM request to provide the location and size of the tisci_boardcfg Resource Man...
Definition: tisci_core.h:126
uint32_t tisci_boardcfg_rmp_high
Definition: tisci_core.h:129
uint8_t abi_major
Definition: tisci_core.h:85
uint32_t tisci_boardcfg_pmp_low
Definition: tisci_core.h:237
devgrp_t tisci_boardcfg_rm_devgrp
Definition: tisci_core.h:131
TISCI_MSG_VERSION request to provide version info about currently running firmware.
Definition: tisci_core.h:81
struct tisci_header hdr
Definition: tisci_core.h:170
TISCI_MSG_QUERY_MSMC request to provide currently available MSMC memory if present in the SoC.
Definition: tisci_core.h:265
uint32_t tisci_boardcfg_securityp_high
Definition: tisci_core.h:205
uint32_t tisci_boardcfgp_low
Definition: tisci_core.h:171
Empty response for TISCI_MSG_BOARD_CONFIG_SECURITY.
Definition: tisci_core.h:218
TISCI_MSG_BOARD_CONFIG_PM request to provide the location and size of the tisci_boardcfg Power Manage...
Definition: tisci_core.h:235
uint8_t devgrp_t
Defines the sysfw DEVGRP type. This is meant to be used in code or data structures that require disti...
Definition: sciclient.h:242
char str[32]
Definition: tisci_core.h:83
struct tisci_header hdr
Definition: tisci_core.h:155
struct tisci_header hdr
Definition: tisci_core.h:236
Response to notification message about firmware availability.
Definition: tisci_core.h:110
struct tisci_header hdr
Definition: tisci_core.h:143
TISCI_MSG_BOARD_CONFIG request to provide the location and size of the tisci_boardcfg structure.
Definition: tisci_core.h:169
uint32_t msmc_start_low
Definition: tisci_core.h:283
uint32_t msmc_end_high
Definition: tisci_core.h:286
uint16_t tisci_boardcfg_rm_size
Definition: tisci_core.h:130
Empty response for TISCI_MSG_BOARD_CONFIG_RM.
Definition: tisci_core.h:142
uint32_t tisci_boardcfg_pmp_high
Definition: tisci_core.h:238
uint32_t msmc_end_low
Definition: tisci_core.h:285
Notification message to indicate the DMSC is available.
Definition: tisci_core.h:97
struct tisci_header hdr
Definition: tisci_core.h:98
struct tisci_header hdr
Definition: tisci_core.h:252
struct tisci_header hdr
Definition: tisci_core.h:266
Empty response for TISCI_MSG_BOARD_CONFIG.
Definition: tisci_core.h:185
Empty response for TISCI_MSG_BOARD_CONFIG_RESASG.
Definition: tisci_core.h:154
uint8_t patch_version
Definition: tisci_core.h:88
uint32_t extboot_status
Definition: tisci_core.h:99
devgrp_t tisci_boardcfg_security_devgrp
Definition: tisci_core.h:207
struct tisci_header hdr
Definition: tisci_core.h:82
devgrp_t tisci_boardcfg_pm_devgrp
Definition: tisci_core.h:240
uint32_t tisci_boardcfg_rmp_low
Definition: tisci_core.h:128
TISCI_MSG_BOARD_CONFIG_SECURITY request to provide the location and size of the tisci_boardcfg securi...
Definition: tisci_core.h:202
struct tisci_header hdr
Definition: tisci_core.h:219
Empty response for TISCI_MSG_BOARD_CONFIG_PM.
Definition: tisci_core.h:251
uint8_t sub_version
Definition: tisci_core.h:87
uint16_t version
Definition: tisci_core.h:84
struct tisci_header hdr
Definition: tisci_core.h:203
struct tisci_header hdr
Definition: tisci_core.h:111
TISCI_MSG_QUERY_MSMC request response providing currently available MSMC memory if present in the SoC...
Definition: tisci_core.h:281
struct tisci_msg_version_req __attribute__((__packed__))
This file contains:
Definition: tisci_core.h:66
uint32_t tisci_boardcfg_securityp_low
Definition: tisci_core.h:204