PDK API Guide for J721E
|
TISCI_MSG_VERSION request to provide version info about currently running firmware.
hdr | TISCI header. |
str | Human readable version string. |
version | Version number of the firmware. |
abi_major | Major version number of ABI in use by firmware. |
abi_minor | Minor version number of ABI in use by firmware. |
sub_version | Sub-version number of the firmware. |
patch_version | Patch-version number of the firmware. |
Data Fields | |
struct tisci_header | hdr |
char | str [32] |
uint16_t | version |
uint8_t | abi_major |
uint8_t | abi_minor |
uint8_t | sub_version |
uint8_t | patch_version |
struct tisci_header tisci_msg_version_resp::hdr |
char tisci_msg_version_resp::str[32] |
uint16_t tisci_msg_version_resp::version |
uint8_t tisci_msg_version_resp::abi_major |
uint8_t tisci_msg_version_resp::abi_minor |
uint8_t tisci_msg_version_resp::sub_version |
uint8_t tisci_msg_version_resp::patch_version |