![]() |
PDK API Guide for J721E
|
Request message for writing to an OTP row.
hdr | Common TI-SCI header |
row_idx | Index of the otp row to be written. Index starts from zero. |
row_val | value to be written to the otp row |
row_mask | mask specifying the bits in row_val to be written |
Data Fields | |
struct tisci_header | hdr |
uint8_t | row_idx |
uint32_t | row_val |
uint32_t | row_mask |
struct tisci_header tisci_msg_write_otp_row_req::hdr |
uint8_t tisci_msg_write_otp_row_req::row_idx |
uint32_t tisci_msg_write_otp_row_req::row_val |
uint32_t tisci_msg_write_otp_row_req::row_mask |