![]() |
PDK API Guide for J721E
|
This file contains:
WARNING!!: Autogenerated file from SYSFW. DO NOT MODIFY!!
System Firmware
TISCI Data structures and macros for processor boot messagesRequest for physical processor control request
Provides a means for either the "recovery master" host or another host in the permitted access list to request for a physical processor control.
hdr | Generic TISCI message header. |
processor_id | Specifies a Processor ID. See the SoC Family Specific Documentation Chapter of the TISCI User Guide for accepted values. |
Data Fields | |
struct tisci_header | hdr |
uint8_t | processor_id |
struct tisci_header tisci_msg_proc_request_req::hdr |
uint8_t tisci_msg_proc_request_req::processor_id |