PDK API Guide for J721E
|
Structure contains the application buffer information to store configuration, which will be written through UDMA.
Data Fields | |
uint32_t * | bufferPtr |
uint32_t | length |
bool | configThroughUdmaFlag |
uint32_t* Vhwa_M2mVissConfigAppBuff::bufferPtr |
< Buffer pointer passed from the application length of application buffer in number of bytes bytes
uint32_t Vhwa_M2mVissConfigAppBuff::length |
configuration through UDMA is enabled or not
bool Vhwa_M2mVissConfigAppBuff::configThroughUdmaFlag |