PDK API Guide for J721E
|
UDMA ring monitor object.
UDMA ring monitor handle.
Note: This is an internal/private driver structure and should not be used or modified by caller.
Data Fields | |
Udma_DrvHandle | drvHandle |
uint16_t | ringMonNum |
uint32_t | ringMonInitDone |
Udma_DrvHandle Udma_RingMonHandle::drvHandle |
Pointer to global driver handle.
uint16_t Udma_RingMonHandle::ringMonNum |
Ring number
uint32_t Udma_RingMonHandle::ringMonInitDone |
Flag to set the ring monitor object is init.