PDK API Guide for J721E
|
UDMA RX channel mapped flow alloc parameters.
Data Fields | |
uint32_t | mappedFlowGrp |
uint32_t | mappedChNum |
uint32_t Udma_FlowAllocMappedPrms::mappedFlowGrp |
The Mapped flow group to use when channel type is UDMA_CH_TYPE_RX_MAPPED.
The driver will allocate mapped flows from this group. Refer Udma_MappedRxGrpSoc macro for details about mapped RX flow groups.
uint32_t Udma_FlowAllocMappedPrms::mappedChNum |
The assigned mapped channel number when channel type is UDMA_CH_TYPE_RX_MAPPED.
This is used to allocate the corresponding mapped flow for the particular channel. The driver will allocate from the mapped flows which are dedicated for this particular channel.