PDK API Guide for J721E
|
H3A Input Configuration structure Used to configure input modules for the H3A Used to select input to the H3A module and also Lut configuration for H3A input.
Data Fields | |
uint32_t | inSel |
uint32_t | shift |
uint32_t Rfe_H3aInConfig::inSel |
uint32_t Rfe_H3aInConfig::shift |
Select input source for H3A, Refer Rfe_H3aInputSelect for valid values U8, number of right shift, from 0 to 14 Used to convert input bit depth to 10bit