PDK API Guide for J721E
|
White Balance configuration Structure Used for white balance correction Used for digital gain to be applied if the image is too dark even after analog gain and exposure time have been set to the maximum. Allows to set gain independently for each channel, the gain value can range from 0 to 31.996 in steps of 1/256.
Data Fields | |
uint32_t | gain [RFE_MAX_COLOR_COMP] |
uint32_t | offset [RFE_MAX_COLOR_COMP] |
uint32_t Rfe_GainOfstConfig::gain[RFE_MAX_COLOR_COMP] |
White balance gain for each pixel in 2x2 format, The gain value at index 0 is applied to even pixel on even line. The gain value at index 1 is applied to odd pixel on even line. The gain value at index 2 is applied to even pixel on odd line. The gain value at index 3 is applied to odd pixel on odd line. in U13Q9 format
uint32_t Rfe_GainOfstConfig::offset[RFE_MAX_COLOR_COMP] |
White balance offset for each pixel in 2x2 format, in S16 format The offset value at index 0 is applied to even pixel on even line. The offset value at index 1 is applied to odd pixel on even line. The offset value at index 2 is applied to even pixel on odd line. The offset value at index 3 is applied to odd pixel on odd line.