PDK API Guide for J721E
|
DPC OTF configuration Structure When both DPC LUT and DPC OTF are enabled, this DPC OTF gets applied after DPC LUT. Automatically detecting the defects based on thresholds and slopes Preferred method when exact location of the defective pixels is not known.
Data Fields | |
uint32_t | enable |
uint32_t | threshold [RFE_DPC_OTF_LUT_SIZE] |
uint32_t | slope [RFE_DPC_OTF_LUT_SIZE] |
uint32_t Rfe_DpcOtfConfig::enable |
Flag to enable/disable DPC OTF module TRUE: Enable this module FALSE: Disables this module When module disabled, it does not update threshold/slope Lut
uint32_t Rfe_DpcOtfConfig::threshold[RFE_DPC_OTF_LUT_SIZE] |
Threshold value
uint32_t Rfe_DpcOtfConfig::slope[RFE_DPC_OTF_LUT_SIZE] |
slope value