PDK API Guide for J721E
|
DPC Lut configuration Structure When both DPC LUT and DPC OTF are enabled, this DPC LUT gets applied first. At max, 256 defective pixels can be corrected using DPC LUT. Used when exact location of the (typically manufacturing )defective pixels are known.
Data Fields | |
uint32_t | enable |
uint32_t | isReplaceWhite |
uint32_t | table [RFE_DPC_LUT_SIZE] |
uint32_t | maxDefectPixels |
uint32_t Rfe_DpcLutConfig::enable |
Flag to enable/disable DPC Lut module TRUE: Enable this module FALSE: Disables this module When module disabled, it does not update Lut
uint32_t Rfe_DpcLutConfig::isReplaceWhite |
When correction method is selected as 0 (replace with white or black color) in LUT, This flag is used to select black or white color TRUE: Replace defect pixel with white color FALSE: Replace detect pixel with black color
uint32_t Rfe_DpcLutConfig::table[RFE_DPC_LUT_SIZE] |
Table containing defect pixel x and y position and correction method
uint32_t Rfe_DpcLutConfig::maxDefectPixels |
Maximum number of detective pixels, ie size of array table must be less than RFE_DPC_LUT_SIZE