PDK API Guide for J721E
|
Data Fields | |
uint16_t | enablecache |
uint16_t | isDataBufferPayloadStructure |
Mcasp_HwSetup | mcaspHwSetup |
uint16_t | pscPwrmEnable |
uint16_t Mcasp_Params::enablecache |
Option to select whether to enable cache or not(default is TRUE)
uint16_t Mcasp_Params::isDataBufferPayloadStructure |
This is useful during the operation of the Mcasp in DIT mode.This parameter indicates if the data buffer has to be interpreted as a payload structure,i.e whether the channel status and user data is also included in the application buffer and hence has to be appropriately interpreted.(Default is FALSE).
Mcasp_HwSetup Mcasp_Params::mcaspHwSetup |
Register information for initialising the Mcasp hardware.
uint16_t Mcasp_Params::pscPwrmEnable |
Option to enable or disable the PSC control in the driver