PDK API Guide for J721E
|
Resource Table Device VRing Structure.
Data Fields | |
uint32_t | da |
uint32_t | align |
uint32_t | num |
uint32_t | notifyid |
uint32_t | reserved |
uint32_t Ipc_VDevVRing::da |
device address
uint32_t Ipc_VDevVRing::align |
Alignment of the buffer.
uint32_t Ipc_VDevVRing::num |
Number of buffers
uint32_t Ipc_VDevVRing::notifyid |
NotifyId for receive channel
uint32_t Ipc_VDevVRing::reserved |
Reserved for future use