PDK API Guide for J721E
|
Structure used for remoteproc trace.
Data Fields | |
uint32_t | type |
uint32_t | da |
uint32_t | len |
uint32_t | reserved |
uint8_t | name [NAME_LEN] |
uint32_t Ipc_Trace::type |
Type of trace
uint32_t Ipc_Trace::da |
Device Address
uint32_t Ipc_Trace::len |
Length of buffer
uint32_t Ipc_Trace::reserved |
Reserved for future use
uint8_t Ipc_Trace::name[NAME_LEN] |
Name of the trace