PDK API Guide for J721E
|
Paxel/Window configuration structure Used to define paxel for AEWB and window for AF.
Data Fields | |
Fvid2_PosConfig | pos |
uint32_t | width |
uint32_t | height |
uint32_t | horzCount |
uint32_t | vertCount |
uint32_t | horzIncr |
uint32_t | vertIncr |
Fvid2_PosConfig H3a_PaxelConfig::pos |
Paxel/Window start Position For AF, Start horizontal position must be iirFiltStartPos + 2 and must be even Start vertical position must be greater than 8 if vertical mode is enabled, range is 0-4095 For AEWB, Start horizontal position must be in 0-4095 Start vertical position must be 0-4095
uint32_t H3a_PaxelConfig::width |
Width of the paxel, minimum width required is 8 pixels
uint32_t H3a_PaxelConfig::height |
Height of the paxel The height could be from 2 to 256
uint32_t H3a_PaxelConfig::horzCount |
Horizontal paxel count, Valid value is from 2 to 36
uint32_t H3a_PaxelConfig::vertCount |
Vertical Paxel count, Maximum value supported is 128
uint32_t H3a_PaxelConfig::horzIncr |
Horizontal increment, The Range is from 2 to 32
uint32_t H3a_PaxelConfig::vertIncr |
Vertical increment, The range is from 2 to 32