PDK API Guide for J721E
|
The definition of a GPIO function table that contains the required set of functions to control a specific GPIO driver implementation.
GPIO_InitFxn GPIO_FxnTable::initFxn |
Function to initialize the given data object
GPIO_ReadFxn GPIO_FxnTable::readFxn |
Function to read from the specified peripheral
GPIO_WriteFxn GPIO_FxnTable::writeFxn |
Function to write from the specified peripheral
GPIO_clearIntFxn GPIO_FxnTable::clearIntFxn |
Function to clear a GPIO pin interrupt flag
GPIO_disableIntFxn GPIO_FxnTable::disableIntFxn |
Function to disable a GPIO pin interrupt flag
GPIO_enableIntFxn GPIO_FxnTable::enableIntFxn |
Function to enable a GPIO pin interrupt flag
GPIO_setCallbackFxn GPIO_FxnTable::setCallbackFxn |
Function to bind a callback function to a GPIO pin interrupt
GPIO_setConfigFxn GPIO_FxnTable::setConfigFxn |
Function to configure the gpio pin
GPIO_toggleFxn GPIO_FxnTable::toggleFxn |
Function to toggles the current state of a GPIO