![]() |
PDK API Guide for J721E
|
FVID2 video buffer format specification.
Used during Fvid2_create() by some drivers. Used as parameter to Fvid2_setFormat(), Fvid2_getFormat() by some drivers.
Data Fields | |
uint32_t | chNum |
uint32_t | width |
uint32_t | height |
uint32_t | pitch [FVID2_MAX_PLANES] |
uint32_t | fieldMerged [FVID2_MAX_PLANES_PER_FIELD] |
uint32_t | dataFormat |
uint32_t | scanFormat |
uint32_t | ccsFormat |
uint32_t Fvid2_Format::chNum |
Channel Number to which this format belongs to.
uint32_t Fvid2_Format::width |
Width of the video frame or field in pixels.
uint32_t Fvid2_Format::height |
Height of the video frame or field in lines.
uint32_t Fvid2_Format::pitch[FVID2_MAX_PLANES] |
Pitch in bytes for each of the sub-buffers. This represents the difference between two consecutive line addresses in bytes. This is irrespective of whether the video is interlaced or progressive and whether the fields are merged or separated for interlaced video.
uint32_t Fvid2_Format::fieldMerged[FVID2_MAX_PLANES_PER_FIELD] |
This field tells whether both the fields have to be merged, i.e line interleaved or not. Used only for interlaced format. The effective pitch is calculated based on this information along with pitch parameter. If fields are merged, effective pitch = pitch * 2 else effective pitch = pitch.
uint32_t Fvid2_Format::dataFormat |
Frame data Format. For valid values see Fvid2_DataFormat.
uint32_t Fvid2_Format::scanFormat |
Scan Format. For valid values see Fvid2_ScanFormat.
uint32_t Fvid2_Format::ccsFormat |
Color Component Storage format. For valid values see Fvid2_ColorCompStorageFmt.