PDK API Guide for J721E
|
Structure for configuring RGB Companding LUT This Lut is used for companding 12b RGB to 8b RGB If this lut is disabled, a fixed shift is used for converting 12b to 8b RGB. There is only one enable bit for all three luts.
Note: There are only 3 Luts physically present and the LUTs are muxed between Y/R, UV/G, Sat/B, so depending on the output selected, configure the companding Luts.
Data Fields | |
uint32_t | enable |
uint32_t * | redLutAddr |
uint32_t * | greenLutAddr |
uint32_t * | blueLutAddr |
uint32_t Fcp_RgbLutConfig::enable |
Used to enable Lut based companding for RGB 12b to 8b conversion All three Lut pointer must not be null when set to TRUE when set to FALSE, shift is used to convert from 12b to 8b
uint32_t* Fcp_RgbLutConfig::redLutAddr |
Pointer to the Lut with 513 entries Used for converting red color from 12b to 8b
uint32_t* Fcp_RgbLutConfig::greenLutAddr |
Pointer to the Lut with 513 entries Used for converting green color from 12b to 8b
uint32_t* Fcp_RgbLutConfig::blueLutAddr |
Pointer to the Lut with 513 entries Used for converting blue color from 12b to 8b