PDK API Guide for J721E
|
There are 5 output channels from VISS, the outputs format for all of them can be selecting appropriate data formats. The data format can further be overridded using below variables. For example, Luma and chroma 12 bit output can be selected by YUV420 data format and 12bit CCSF, luma12 output channel can further be changed to get Greyscale value from RGB2HSV output using Fcp_Luma12OutSelect in the below structure.
Data Fields | |
uint32_t | luma12OutSel |
uint32_t | chroma12OutSel |
uint32_t | luma8OutSel |
uint32_t | chroma8OutSel |
uint32_t | sat8OutSel |
uint32_t | chromaMode |
uint32_t Fcp_OutputSelect::luma12OutSel |
Select output on Luma12b output channel, Refer Fcp_Luma12OutSelect for valid values
uint32_t Fcp_OutputSelect::chroma12OutSel |
Select output on Chroma12b output channel, Refer Fcp_Chroma12OutSelect for valid values
uint32_t Fcp_OutputSelect::luma8OutSel |
Select output on Luma8b output channel, Refer Fcp_Luma8OutSelect for valid values
uint32_t Fcp_OutputSelect::chroma8OutSel |
Select output on Chroma8b output channel, Refer Fcp_Chroma8OutSelect for valid values
uint32_t Fcp_OutputSelect::sat8OutSel |
Select output on Saturation output channel, Refer Fcp_Sat8OutSelect for valid values
uint32_t Fcp_OutputSelect::chromaMode |
Used to select 420 or 422 output, Refer Fcp_ChromaMode for valid values.